<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 PE &amp; Round Robin  MQX</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412509#M3090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use MQX in round robin tasks.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use Processor Expert PE to generate the MQX tasks using the OS_Task component, &lt;/P&gt;&lt;P&gt;the PE overwrites the MQX_TIME_SLICE_TASK attribute and the tasks time slice value.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Is there any way to make PE set these values so every time&amp;nbsp; I run the PE I don't need to manually go and type in these values?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Aug 2015 00:40:47 GMT</pubDate>
    <dc:creator>aussiemate</dc:creator>
    <dc:date>2015-08-05T00:40:47Z</dc:date>
    <item>
      <title>PE &amp; Round Robin  MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412509#M3090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use MQX in round robin tasks.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use Processor Expert PE to generate the MQX tasks using the OS_Task component, &lt;/P&gt;&lt;P&gt;the PE overwrites the MQX_TIME_SLICE_TASK attribute and the tasks time slice value.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Is there any way to make PE set these values so every time&amp;nbsp; I run the PE I don't need to manually go and type in these values?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 00:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412509#M3090</guid>
      <dc:creator>aussiemate</dc:creator>
      <dc:date>2015-08-05T00:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: PE &amp; Round Robin  MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412510#M3091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matthew,&lt;/P&gt;&lt;P&gt;I do not see a way to set up the TIMESLICE within PE.&lt;/P&gt;&lt;P&gt;If you have multiple tasks with the same priority level, then they are going to round robin.&amp;nbsp; You just need to make sure there is some code in each task that will block it (ex: OSA_TimeDelay) so the other task will get a chance to run.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 21:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412510#M3091</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-08-05T21:45:07Z</dc:date>
    </item>
    <item>
      <title>Re: PE &amp; Round Robin  MQX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412511#M3092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK,&lt;/P&gt;&lt;P&gt;will have a look at the non time sliced same priority method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just assumed that PE would have some method of enabling time slicing using the MQX_TIME_SLICE_TASK parameter without destroying the manually edited values each time...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 03:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/PE-Round-Robin-MQX/m-p/412511#M3092</guid>
      <dc:creator>aussiemate</dc:creator>
      <dc:date>2015-08-10T03:40:26Z</dc:date>
    </item>
  </channel>
</rss>