<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Do I need KSDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411870#M3048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ernest,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which chip do you use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the PE and SDK+PE ，&amp;nbsp; you can consider like this : There are two frameworks PE and KSDK+PE, the two PE are difference , they have no relationship.&lt;/P&gt;&lt;P&gt;The former PE almost the same as the PE on CW; the KSDK+PE is a&amp;nbsp; new one .&lt;/P&gt;&lt;P&gt;Some chips only support the KSDK , for in the future , all the kinetis chips will support the KSDK .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Oct 2015 01:47:39 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2015-10-20T01:47:39Z</dc:date>
    <item>
      <title>Do I need KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411869#M3047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the past I used CW &amp;amp; Processor Expert to build a framework on Coldfire MCUs for projects which worked out very successfully. Now I plan to do the same with Kinetis for a range of new projects (for the time being I do not plan to use an OS) and use PE to get up and running quickly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having briefly looked through a few docs for KSDK and KDS, I think I do not need to install KSDK, can someone correct me if I am wrong.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone also explain why the PE functionality appears to be duplicated in KSDK? It all seems a bit confusing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 19:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411869#M3047</guid>
      <dc:creator>therealfreegeek</dc:creator>
      <dc:date>2015-10-19T19:35:33Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411870#M3048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ernest,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which chip do you use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the PE and SDK+PE ，&amp;nbsp; you can consider like this : There are two frameworks PE and KSDK+PE, the two PE are difference , they have no relationship.&lt;/P&gt;&lt;P&gt;The former PE almost the same as the PE on CW; the KSDK+PE is a&amp;nbsp; new one .&lt;/P&gt;&lt;P&gt;Some chips only support the KSDK , for in the future , all the kinetis chips will support the KSDK .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 01:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411870#M3048</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-10-20T01:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411871#M3049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice, thanks for responding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will probably start with the K26. As I have many projects and the price of the MCU is not important, a super-set device would be flexible for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really like the conventional PE, it is vary sad to see that it will be phased out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 12:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411871#M3049</guid>
      <dc:creator>therealfreegeek</dc:creator>
      <dc:date>2015-10-20T12:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: Do I need KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411872#M3050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ernest,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for maybe i cause misunderstanding to you .&lt;/P&gt;&lt;P&gt;The KSDK also can through configure the PE to development :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/23911i051351C11DE92DC4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 02:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Do-I-need-KSDK/m-p/411872#M3050</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-10-21T02:23:25Z</dc:date>
    </item>
  </channel>
</rss>