<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401575#M2691</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now working on our own board and passed the FRDM-K64 development board.&amp;nbsp; I see that PE would not be able&lt;/P&gt;&lt;P&gt;to make this happen, since, the PINs are mux.&amp;nbsp; So I would have to dynamically, set &amp;amp; release UART3 depending on &lt;/P&gt;&lt;P&gt;the pins I would like to communicate on using the UART3.&amp;nbsp; Your are right it is pins 5&amp;amp;6, I should use a ruler when trying&lt;/P&gt;&lt;P&gt;to isolate the pins on the schematic....LOL.....not as young as I used to be....LOL!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to see how PE sets UART3 for one, then I know how to set the other, when I try to do it dynamically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2015 20:18:36 GMT</pubDate>
    <dc:creator>neilporven</dc:creator>
    <dc:date>2015-06-16T20:18:36Z</dc:date>
    <item>
      <title>Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401571#M2687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't access the multiple UART3 using PE? PE is saying there is conflict although there are several&lt;/P&gt;&lt;P&gt;UART3 On the K64?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 02:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401571#M2687</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-06-16T02:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401572#M2688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;Yes, it can not use two same UART.&lt;/P&gt;&lt;P&gt;And why you want use two UART3? what function do you want to realize ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 02:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401572#M2688</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-06-16T02:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401573#M2689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The function is a SCI communication.&amp;nbsp; The uP has multiple UART3 on PINs (58_RX,59_TX, 90_Rx, 91_TX, 6_RX, 7_TX), my &lt;/P&gt;&lt;P&gt;hardware is already connected to this PINs.&amp;nbsp; Is there a way to use UART3 on these pins, either through PE or time share it and &lt;/P&gt;&lt;P&gt;configure it outside of PE manually?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 12:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401573#M2689</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-06-16T12:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401574#M2690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Neil,&lt;/P&gt;&lt;P&gt;We mux the peripherals to multiple pins to enable a wide range of configurations (i.e. we have more capability on-chip than pins allow so we mux and let you choose what pins to have the peripheral capability come out on).&lt;/P&gt;&lt;P&gt;Now you cannot have the UART3 connected to more than one set of pins simultaneously.&amp;nbsp; Yes you could dynamically change this.&amp;nbsp; It just is not a typical application.&lt;/P&gt;&lt;P&gt;You need to be sure other application code is not trying to use those pins as well (i.e. avoid contention).&lt;/P&gt;&lt;P&gt;Once you have played around, feel free to post your project.&lt;/P&gt;&lt;P&gt;Are you using the freedom or tower hardware for development?&amp;nbsp; If yes, that makes life much easier for us to help support.&lt;/P&gt;&lt;P&gt;Please note I looked at the reference manual for the 100-pin and see a difference:&lt;/P&gt;&lt;P&gt;UART_TX/RX on pins 5&amp;amp;6....not 6&amp;amp;7.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 15:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401574#M2690</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-06-16T15:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401575#M2691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now working on our own board and passed the FRDM-K64 development board.&amp;nbsp; I see that PE would not be able&lt;/P&gt;&lt;P&gt;to make this happen, since, the PINs are mux.&amp;nbsp; So I would have to dynamically, set &amp;amp; release UART3 depending on &lt;/P&gt;&lt;P&gt;the pins I would like to communicate on using the UART3.&amp;nbsp; Your are right it is pins 5&amp;amp;6, I should use a ruler when trying&lt;/P&gt;&lt;P&gt;to isolate the pins on the schematic....LOL.....not as young as I used to be....LOL!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to see how PE sets UART3 for one, then I know how to set the other, when I try to do it dynamically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 20:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401575#M2691</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-06-16T20:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert, UART3, and MK64Fxx 100pin LQFP</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401576#M2692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On PE , if&amp;nbsp; you want use one pin to two function , you can use "ConnectPin" method .&lt;/P&gt;&lt;P&gt;For example , PTE5 used to GPIO and the Receiver of UART3, do like this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61136i158AFB9A110ABEFC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then, &lt;SPAN style="font-size: 12.0pt; font-family: 'Times New Roman','serif';"&gt;. You can use ConnectPin() method of BitIO and Serial_LDD to switch the routing at runtime. &lt;BR /&gt; &lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61138i4D87813A368CB9EA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Times New Roman','serif';"&gt;Hope it helps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Times New Roman','serif';"&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Times New Roman','serif';"&gt;Alice&lt;BR /&gt; &lt;/SPAN&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 09:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Processor-Expert-UART3-and-MK64Fxx-100pin-LQFP/m-p/401576#M2692</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-07-01T09:31:26Z</dc:date>
    </item>
  </channel>
</rss>