<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Best way to change processor memory variant? in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400132#M2633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick reply, and sorry for the double post.&amp;nbsp; I assumed incorrectly that I did something wrong on the first one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That solution looks good.&amp;nbsp; It would be really helpful in the future if it were a little easier to move between memory sizes.&amp;nbsp; Having to manually re-enter the PE config information is time consuming and could result in errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feel free to delete the other duplicate thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Apr 2015 12:11:35 GMT</pubDate>
    <dc:creator>LI_Dave</dc:creator>
    <dc:date>2015-04-12T12:11:35Z</dc:date>
    <item>
      <title>Best way to change processor memory variant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400130#M2631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have&amp;nbsp; project on a KL05Z8 and want to move to a larger memory version such as the MKL05Z32.&amp;nbsp; There doesn't seem to be a simple way to do this.&amp;nbsp; PE lets you change package types, but not memory sizes.&amp;nbsp; Am I missing something?&amp;nbsp; I suppose I could just edit the ROM/RAM areas in the CPU component inspector, but that seems inelegant.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Apr 2015 21:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400130#M2631</guid>
      <dc:creator>LI_Dave</dc:creator>
      <dc:date>2015-04-11T21:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: Best way to change processor memory variant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400131#M2632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello LI_Dave:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can add the processor from &lt;EM&gt;Components Library -&amp;gt; Processors:&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49321i50691C81C08A8577/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The wizard will prompt you to select the package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyalert: The wizard will also ask you about the compiler. Make sure that &lt;STRONG&gt;GNU C Compiler&lt;/STRONG&gt; is selected, since it is the one used by KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49424i7D1AD01CA626D4B7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyinfo: The drawback is that you need to replicate the CPU settings in this new component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can choose to remove the previous CPU or leave it so you can jump back to that one if you wish using the context menu -&amp;gt; Component Enabled:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49479i04DD822914882249/image-size/large?v=v2&amp;amp;px=999" title="CPU_Enable.png" alt="CPU_Enable.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Apr 2015 03:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400131#M2632</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-04-12T03:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: Best way to change processor memory variant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400132#M2633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick reply, and sorry for the double post.&amp;nbsp; I assumed incorrectly that I did something wrong on the first one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That solution looks good.&amp;nbsp; It would be really helpful in the future if it were a little easier to move between memory sizes.&amp;nbsp; Having to manually re-enter the PE config information is time consuming and could result in errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feel free to delete the other duplicate thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Apr 2015 12:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Best-way-to-change-processor-memory-variant/m-p/400132#M2633</guid>
      <dc:creator>LI_Dave</dc:creator>
      <dc:date>2015-04-12T12:11:35Z</dc:date>
    </item>
  </channel>
</rss>