<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: SDK RTOS Abstraction</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313976#M248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich for your quickly response. It's great for mixing use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jun 2014 09:24:29 GMT</pubDate>
    <dc:creator>matherinewang</dc:creator>
    <dc:date>2014-06-05T09:24:29Z</dc:date>
    <item>
      <title>SDK RTOS Abstraction</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313974#M246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SDK supports RTOS Abstraction Layer, it seems that if i use SDK, then i must use abstraction API instead of the RTOS API, such as use task_create() instead of xTaskCreate() in freeRTOS, is it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I still want to use freeRTOS API in KDS,&amp;nbsp; can KDS supports freeRTOS awareness now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 02:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313974#M246</guid>
      <dc:creator>matherinewang</dc:creator>
      <dc:date>2014-06-04T02:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: SDK RTOS Abstraction</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313975#M247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You still can use the RTOS API, in fact you can even mix the SDK RTOS and the normal RTOS API in parallel (at least for FreeRTOS, I'm using it in that way).&lt;/P&gt;&lt;P&gt;Not using the SDK RTOS API has the advantage that it does not add an additional layer (faster and less code).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And yes, with KDS you can use the FreeRTOS kernel awarness. You only need to download the Wittenstein plugins. See &lt;A href="http://mcuoneclipse.com/2013/08/04/diy-free-toolchain-for-kinetis-part-5-freertos-eclipse-kernel-awareness-with-gdb/" title="http://mcuoneclipse.com/2013/08/04/diy-free-toolchain-for-kinetis-part-5-freertos-eclipse-kernel-awareness-with-gdb/"&gt;http://mcuoneclipse.com/2013/08/04/diy-free-toolchain-for-kinetis-part-5-freertos-eclipse-kernel-awareness-with-gdb/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Just make sure you are using the 'OpenRTOS (DSF)' views with KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 18:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313975#M247</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-06-04T18:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: SDK RTOS Abstraction</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313976#M248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich for your quickly response. It's great for mixing use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 09:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/SDK-RTOS-Abstraction/m-p/313976#M248</guid>
      <dc:creator>matherinewang</dc:creator>
      <dc:date>2014-06-05T09:24:29Z</dc:date>
    </item>
  </channel>
</rss>