<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: KDS Code generator failure</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Code-generator-failure/m-p/313787#M245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the problem is that you are using a component (ADC) from the set of High-level components that are not compatible with SDK library. &lt;/P&gt;&lt;P&gt;The High level components cannot be combined in one project with components using Kinetis SDK (starting with fsl_).&lt;/P&gt;&lt;P&gt;So if you select to use SDK in the project creation wizard, you need to use only fsl_... component and vice versa if you don't use SDK you cannot use fsl_ ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, there is a defect in the beta release that the Components library view shows the high level components even in SDK project which is not correct.&lt;/P&gt;&lt;P&gt;This will be fixed for next release. A workaround is to use a proper type of component for the particular type of project (SDK/non-SDK).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It has been already mentioned in &lt;A href="https://community.nxp.com/message/407946"&gt;Re: KDS - Processor Expert for PWMs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jul 2014 13:25:17 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2014-07-14T13:25:17Z</dc:date>
    <item>
      <title>KDS Code generator failure</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Code-generator-failure/m-p/313786#M244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build a simple ADC project (after epic fail on large design) for an MK64FN1M0VLQ12, but KDS is not able to generate the code. I am receiving a "Generator: FAILURE: Unexpected status of script: Drivers\Kinetis\ADC_NO_FIFO.drv, please contact Freescale support." message. The only components are the pin settings and the 2 ADC modules.&lt;/P&gt;&lt;P&gt;I have attached a zip of the project.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338857"&gt;new2.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 13:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Code-generator-failure/m-p/313786#M244</guid>
      <dc:creator>smiller</dc:creator>
      <dc:date>2014-06-30T13:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: KDS Code generator failure</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Code-generator-failure/m-p/313787#M245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the problem is that you are using a component (ADC) from the set of High-level components that are not compatible with SDK library. &lt;/P&gt;&lt;P&gt;The High level components cannot be combined in one project with components using Kinetis SDK (starting with fsl_).&lt;/P&gt;&lt;P&gt;So if you select to use SDK in the project creation wizard, you need to use only fsl_... component and vice versa if you don't use SDK you cannot use fsl_ ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, there is a defect in the beta release that the Components library view shows the high level components even in SDK project which is not correct.&lt;/P&gt;&lt;P&gt;This will be fixed for next release. A workaround is to use a proper type of component for the particular type of project (SDK/non-SDK).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It has been already mentioned in &lt;A href="https://community.nxp.com/message/407946"&gt;Re: KDS - Processor Expert for PWMs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 13:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Code-generator-failure/m-p/313787#M245</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-07-14T13:25:17Z</dc:date>
    </item>
  </channel>
</rss>