<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: commonreginitialization.prg</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393257#M2420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;KDS 3.2. &amp;nbsp;After I setup a new clean project and add the uart_init, I found it is related with the setting of uart interrupt, only the int0 works well.&lt;/P&gt;&lt;P&gt;I have made a post here&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/440902"&gt;https://community.nxp.com/thread/440902&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I will study it for more.&lt;/P&gt;&lt;P&gt;If you have any information , please be kind to told us. thanks ~&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 02:07:18 GMT</pubDate>
    <dc:creator>zhaowum</dc:creator>
    <dc:date>2016-12-15T02:07:18Z</dc:date>
    <item>
      <title>commonreginitialization.prg</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393253#M2416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wasn't the only one with this problem, I know by looking at past posts.&amp;nbsp; There was never a satisfactory answer provided so I did some experimentation.&amp;nbsp; I found that I got the error message about the CommonRegInitialization.prg file with certain settings.&amp;nbsp; I am trying to use the analog slider on a FRDMKE02 board with no luck so far.&amp;nbsp; I have code which compiles, but does not do anything.&amp;nbsp; I decided to use Freemaster.&amp;nbsp; When I use SCI and assign UART1, then I get the error with CommonRegInitialization.prg.&amp;nbsp; There is a partial path provided in the error message.&amp;nbsp; There are two paths in the KDS_3.0.0 directory which match the partial path.&amp;nbsp; In each one I placed a Default_RTOSAdapter.prg which I renamed to CommonRegInitialization.prg.&amp;nbsp; The first path had no effect.&amp;nbsp; The second path, KDS_3.0.0\eclipse\ProcessorExpert\repositories\Drivers\Common did have an effect.&amp;nbsp; When I placed the renamed file in that location, Processor Expert was able to complete.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My request is for the 'Real' CommonRegInitialization.prg file.&amp;nbsp; I don't know what I have now in the generated code and want to have the correct code.&amp;nbsp; I am sure that when I have the correct file in that place, I will then be able to proceed to the next issue.&amp;nbsp; Thanks in advance!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Nov 2015 06:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393253#M2416</guid>
      <dc:creator>andyvoss</dc:creator>
      <dc:date>2015-11-07T06:57:15Z</dc:date>
    </item>
    <item>
      <title>Re: commonreginitialization.prg</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393254#M2417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you post your project so we can test this problem on our side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Enginee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Nov 2015 01:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393254#M2417</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2015-11-11T01:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: commonreginitialization.prg</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393255#M2418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the same problem, Please contact me on zwm(a.t)brosen.com.cn so that I can email you the packed project. Thanks for your kindly help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BW.&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 14:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393255#M2418</guid>
      <dc:creator>zhaowum</dc:creator>
      <dc:date>2016-12-14T14:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: commonreginitialization.prg</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393256#M2419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zona,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which KDS version are you using? If the project cannot be shared in the community I would recommend you to enter a support ticket here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://nxpcommunity.force.com/community/communityLogin?pagename=CommunityContextPage" title="https://nxpcommunity.force.com/community/communityLogin?pagename=CommunityContextPage"&gt;NXP TechSupport Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 15:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393256#M2419</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-12-14T15:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: commonreginitialization.prg</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393257#M2420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;KDS 3.2. &amp;nbsp;After I setup a new clean project and add the uart_init, I found it is related with the setting of uart interrupt, only the int0 works well.&lt;/P&gt;&lt;P&gt;I have made a post here&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/440902"&gt;https://community.nxp.com/thread/440902&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I will study it for more.&lt;/P&gt;&lt;P&gt;If you have any information , please be kind to told us. thanks ~&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;/Zona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 02:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/commonreginitialization-prg/m-p/393257#M2420</guid>
      <dc:creator>zhaowum</dc:creator>
      <dc:date>2016-12-15T02:07:18Z</dc:date>
    </item>
  </channel>
</rss>