<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: How can I Use KDS to setup a MQX project</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310799#M237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to get the "hello2"project to work on a twr60n512 in KDS. I have tried building the libraries according to the MQX_GNU_Getting_Started.pdf guide (editting the mak files to accept gcc_arm v4.8.0 instead of v4.7.4 include paths), then importing these libraries into KDS and building the hello2 source again them, but I'm getting multiple errors.&lt;/P&gt;&lt;P&gt;I used the KDS Toolchain "C:\Freescale\KDS_1.0.1\toolchain" for the builds and ran the .bat scripts provided&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached the lib folder I created, I'm not experienced with library building, so if you could check if it looks alright at a glance or maybe post an example KDS-built library it would be very much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Few things i've noticed:&lt;/P&gt;&lt;P&gt;1) no linker file in gcc_arm build folder (there was in the cdw folder)&lt;/P&gt;&lt;P&gt;2) gcc_arm bsp.a and psp.a are &amp;lt;1.5mb each, whereas the cdw ones are&amp;nbsp; 66mb and 54mb respectively.&lt;/P&gt;&lt;P&gt;3) i'm getting lots of undefined references to '__zero_table_start__' and '__zero_table_end__' (amongst others) from the psp.a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Rael S-R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jul 2014 11:24:08 GMT</pubDate>
    <dc:creator>raels-r</dc:creator>
    <dc:date>2014-07-15T11:24:08Z</dc:date>
    <item>
      <title>How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310795#M233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I want to build a MQX based project,&amp;nbsp; when use KDS, found there is no a wizzard&amp;nbsp; to new the MQX project like CodeWarrior10.X, &lt;BR /&gt;So, how can i do to new a MQX project in KDS ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 04:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310795#M233</guid>
      <dc:creator>yifangguo-b4310</dc:creator>
      <dc:date>2014-06-03T04:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310796#M234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yifang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i think below two thread should answer your questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="11213" data-containertype="14" data-objectid="400328" data-objecttype="2" href="https://community.freescale.com/message/400328#400328"&gt;https://community.freescale.com/message/400328#400328&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="11213" data-containertype="14" data-objectid="100440" data-objecttype="102" href="https://community.freescale.com/docs/DOC-100440"&gt;https://community.freescale.com/docs/DOC-100440&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=================================================&lt;/P&gt;&lt;P&gt;this answer is for you. if it helps, please click on "correct answer" button. thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Zhang Jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 09:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310796#M234</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-06-03T09:10:13Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310797#M235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one thing i'd point out is that while you can't yet use the full MQX you can use processor expert to add MQX Lite support and configure it from the UI. seems to work well for me once i figured out that you can expand the MQX lite component in the 'components' window to manage individual tasks (change name, configure FP support, change stack size, rename the task, etc...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only problem i've had so far is with tasks in the template list that were not marked as&amp;nbsp; MQX_AUTO_START_TASK, see &lt;A href="https://community.nxp.com/thread/324757"&gt;mqxlite problem starting template tasks that were not marked as MQX_AUTO_START_TASK&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 15:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310797#M235</guid>
      <dc:creator>markschuck</dc:creator>
      <dc:date>2014-06-03T15:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310798#M236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As mentioned in the threads that Zhang Jun provided, MQX does not have official support in KDS yet.&amp;nbsp; We are now planning it with new MQX releases coming around August.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can still build existing MQX examples with KDS today using existing GNU tools support already in MQX RTOS.&amp;nbsp; This worked for me.&amp;nbsp; I can not guarantee that it will work for you, but you can try.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Check out section &lt;STRONG&gt;3&lt;/STRONG&gt; &lt;STRONG&gt;Using MQX Makefiles with Eclipse&lt;/STRONG&gt; in the &lt;STRONG&gt;MQX_GNU_Getting_Started.pdf&lt;/STRONG&gt; document in the /doc/tools/gnu folder in MQX RTOS files&amp;nbsp; (e.g. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;C:\Freescale\Freescale_MQX_4_1\doc\tools\gnu).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This section describes creating a new project in Eclipse and using the existing make files to build MQX libraries and examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Mac L&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 15:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310798#M236</guid>
      <dc:creator>macl</dc:creator>
      <dc:date>2014-06-03T15:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310799#M237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to get the "hello2"project to work on a twr60n512 in KDS. I have tried building the libraries according to the MQX_GNU_Getting_Started.pdf guide (editting the mak files to accept gcc_arm v4.8.0 instead of v4.7.4 include paths), then importing these libraries into KDS and building the hello2 source again them, but I'm getting multiple errors.&lt;/P&gt;&lt;P&gt;I used the KDS Toolchain "C:\Freescale\KDS_1.0.1\toolchain" for the builds and ran the .bat scripts provided&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached the lib folder I created, I'm not experienced with library building, so if you could check if it looks alright at a glance or maybe post an example KDS-built library it would be very much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Few things i've noticed:&lt;/P&gt;&lt;P&gt;1) no linker file in gcc_arm build folder (there was in the cdw folder)&lt;/P&gt;&lt;P&gt;2) gcc_arm bsp.a and psp.a are &amp;lt;1.5mb each, whereas the cdw ones are&amp;nbsp; 66mb and 54mb respectively.&lt;/P&gt;&lt;P&gt;3) i'm getting lots of undefined references to '__zero_table_start__' and '__zero_table_end__' (amongst others) from the psp.a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Rael S-R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 11:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310799#M237</guid>
      <dc:creator>raels-r</dc:creator>
      <dc:date>2014-07-15T11:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310800#M238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MQX uses its own linker files, not linker files included by KDS.&amp;nbsp; Sounds like the problem might be related to the linker file you have selected.&amp;nbsp; Coming next month, MQX will officially support KDS, so from then on this will be supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 15:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310800#M238</guid>
      <dc:creator>macl</dc:creator>
      <dc:date>2014-07-15T15:34:49Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310801#M239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Edit: I've since discovered it was some sort of corruption as the folder '..\mqx\source\bsp\twrk60n512\&lt;STRONG&gt;gcc_arm'&lt;/STRONG&gt; was missing, along with 'initflash.ld'.&lt;/P&gt;&lt;P&gt;After copying them from a more complete installation the build was fine and I have since managed to build and debug 'hello2' using the gcc_arm toolchain in KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've tried building the library for the twrk40d100m using the make files and gcc_arm and the linker file was correctly created. Any ideas why the twrk60 linker isn't being made?&lt;/P&gt;&lt;P&gt;I've jumped ship and moved to the twr40 build to try and get this code to atleast build, before trying to sort out issues with the twr60 build.&lt;/P&gt;&lt;P&gt;Had to change a few directories in the make files:&lt;/P&gt;&lt;P&gt;- '/4.7.4/' to '/4.8.0/'&lt;/P&gt;&lt;P&gt;- removed '/armv7e-m/' from directory paths&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The build scripts seem a bit happier after this, but I can't locate a 'libnosys.a' in the KDS toolchain, any ideas where it might be lurking?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I realise that MQX support will be coming to MQX at some point in late August, but i'm currently interning at Freescale Aylesbury, where they've asked me to rebuild one of their MQX demos in KDS and I'll have likely finished my internship by the time the support is released.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rael S-R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310801#M239</guid>
      <dc:creator>raels-r</dc:creator>
      <dc:date>2014-07-16T12:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310802#M240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried building Freescale_MQX_4_1_LINUX_beta as described in &lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;section &lt;STRONG style="font-style: inherit; font-family: inherit;"&gt;3&lt;/STRONG&gt; &lt;STRONG style="font-style: inherit; font-family: inherit;"&gt;Using MQX Makefiles with Eclipse&lt;/STRONG&gt; in the &lt;STRONG style="font-style: inherit; font-family: inherit;"&gt;MQX_GNU_Getting_Started.pdf&lt;/STRONG&gt; document in the /doc/tools/gnu folder in MQX RTOS files&amp;nbsp; (e.g.&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;C:\Freescale\Freescale_MQX_4_1\doc\tools\gnu) as you suggested above. I extracted it so that it resides in /opt/Freescale/Freescale_MQX_4_1_LINUX_beta/ alongside KDS_1.0.1. I edited build/common/make/global.mak and set TOOLCHAIN_ROOTDIR = /opt/Freescale/KDS_1.0.1/toolchain. I then:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;cd /opt/Freescale/Freescale_MQX_4_1_LINUX_beta/build/twrk21d50m/make&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;./build_gcc_arm.sh&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;I get repeated "No such file or directory" errors associated with stdbool.h included from psptypes.h like so:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;make: *** [/opt/Freescale/Freescale_MQX_4_1_LINUX_beta/lib/twrk21d50m.gcc_arm/release/bsp/obj/adc_kadc.o] Error 1&lt;/P&gt;&lt;P&gt;In file included from /opt/Freescale/Freescale_MQX_4_1_LINUX_beta/mqx/source/include/mqx.h:82:0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; from /opt/Freescale/Freescale_MQX_4_1_LINUX_beta/mqx/source/io/adc/kadc/adt_kpdb.c:27:&lt;/P&gt;&lt;P&gt;/opt/Freescale/Freescale_MQX_4_1_LINUX_beta/mqx/source/psp/cortex_m/psptypes.h:29:21: fatal error: stdbool.h: No such file or directory&lt;/P&gt;&lt;P&gt; #include &amp;lt;stdbool.h&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ^&lt;/P&gt;&lt;P&gt;compilation terminated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help,&lt;/P&gt;&lt;P&gt;WMK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 19:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310802#M240</guid>
      <dc:creator>intractablesubt</dc:creator>
      <dc:date>2014-07-28T19:42:35Z</dc:date>
    </item>
    <item>
      <title>Re: How can I Use KDS to setup a MQX project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310803#M241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may have resolved this, but I'm leaving this here for anyone else who hits this.&amp;nbsp; Freescale hard coded the compiler version into the MQX make files.&amp;nbsp; What this means is that you use any gcc toolchain other than 4.8.3, it will fail to find header files.&amp;nbsp; Just update the appropriate gcc_arm.mak file with the compiler version you are using.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 21:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-Use-KDS-to-setup-a-MQX-project/m-p/310803#M241</guid>
      <dc:creator>kalden_srcinc</dc:creator>
      <dc:date>2014-12-03T21:40:27Z</dc:date>
    </item>
  </channel>
</rss>