<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Custom linkage when using Processor Expert</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390818#M2359</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been using a modified linker file on a project.&amp;nbsp; One thing that's a little painful is I have to keep "Freeze Code Generation" turned on to keep it from overwriting my linker file.&amp;nbsp; The other painful thing is if I have to make a change in Processor Expert, I have to enable code generation again, make a backup copy of my linker file, let it overwrite the linker file when it builds, let it fail to build because the linker doesn't know what to do with the sections I've defined, turn off the code generation, copy my linker file back over, then build again.&amp;nbsp; Is there some way to either tell Processor Expert to preserve the linker file, or add your own linker directives?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2015 15:49:28 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2015-01-07T15:49:28Z</dc:date>
    <item>
      <title>Custom linkage when using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390818#M2359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been using a modified linker file on a project.&amp;nbsp; One thing that's a little painful is I have to keep "Freeze Code Generation" turned on to keep it from overwriting my linker file.&amp;nbsp; The other painful thing is if I have to make a change in Processor Expert, I have to enable code generation again, make a backup copy of my linker file, let it overwrite the linker file when it builds, let it fail to build because the linker doesn't know what to do with the sections I've defined, turn off the code generation, copy my linker file back over, then build again.&amp;nbsp; Is there some way to either tell Processor Expert to preserve the linker file, or add your own linker directives?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 15:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390818#M2359</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-01-07T15:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Custom linkage when using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390819#M2360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to set the Generate linker file to NO in the Build options tab of the CPU component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48991iD2161942CB134D01/image-size/large?v=v2&amp;amp;px=999" title="linker file code generation.jpg" alt="linker file code generation.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 17:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390819#M2360</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-01-07T17:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: Custom linkage when using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390820#M2361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!&amp;nbsp; Did not know about that setting.&amp;nbsp; That works perfectly!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 17:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/390820#M2361</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-01-07T17:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: Custom linkage when using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/1916713#M10256</link>
      <description>&lt;P&gt;This option does not appear to exist anymore.&amp;nbsp;&lt;BR /&gt;How can I turn this off in&amp;nbsp;S32 Design Studio for Power Architecture 2.1?&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 01:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Custom-linkage-when-using-Processor-Expert/m-p/1916713#M10256</guid>
      <dc:creator>MESOLAndre</dc:creator>
      <dc:date>2024-07-25T01:29:22Z</dc:date>
    </item>
  </channel>
</rss>