<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 kds 2.0.0 - processor expert - K22FN512LH12 error</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384376#M2178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting the error as seen in the image when creating a processor expert project for the mk22fn512lh12 as is on the FRDM-k22f board. first error: "Error in the inherited component settings ".&amp;nbsp; See attached image for follow on errors.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have installed KDS 2.0, SDK 1.1.1 and SDK and processor expert updates for eclipse as well.&amp;nbsp; I have also esured that I have built the platfromxx.a library for the k22f MCU.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It appears that there some incompatiblity with the k22f and the installed hal libraries.&amp;nbsp; Am I doing something wrong or is the given device truly imcompatilbe with the latest processor expert?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Jan 2015 00:50:11 GMT</pubDate>
    <dc:creator>mjg8t</dc:creator>
    <dc:date>2015-01-04T00:50:11Z</dc:date>
    <item>
      <title>kds 2.0.0 - processor expert - K22FN512LH12 error</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384376#M2178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting the error as seen in the image when creating a processor expert project for the mk22fn512lh12 as is on the FRDM-k22f board. first error: "Error in the inherited component settings ".&amp;nbsp; See attached image for follow on errors.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have installed KDS 2.0, SDK 1.1.1 and SDK and processor expert updates for eclipse as well.&amp;nbsp; I have also esured that I have built the platfromxx.a library for the k22f MCU.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It appears that there some incompatiblity with the k22f and the installed hal libraries.&amp;nbsp; Am I doing something wrong or is the given device truly imcompatilbe with the latest processor expert?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 00:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384376#M2178</guid>
      <dc:creator>mjg8t</dc:creator>
      <dc:date>2015-01-04T00:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: kds 2.0.0 - processor expert - K22FN512LH12 error</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384377#M2179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi M J,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you attach your project , then we can reproduce the error quickly and find the solution as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 01:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384377#M2179</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-01-04T01:34:48Z</dc:date>
    </item>
    <item>
      <title>Re: kds 2.0.0 - processor expert - K22FN512LH12 error</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384378#M2180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fortunately I ran accross Erich Stygers excellent webpage and guide on running the FRDM-K22f with processor expert here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/12/27/usb-with-the-freescale-frdm-k22f-board/" title="http://mcuoneclipse.com/2014/12/27/usb-with-the-freescale-frdm-k22f-board/"&gt;USB with the Freescale FRDM-K22F Board | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The guide indicated that there is an additional Processor Expert K22F update for eclipse needed that is NOT currently listed on teh KDS2.0 updates list here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE&amp;amp;nodeId=0152101E8C1EB4&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE&amp;amp;nodeId=0152101E8C1EB4&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Kinetis Design Studio Integrated Development |Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Hopefully freescale can add the udpate here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So, in short after finding and running the update that is available from the link listed by Erich and updating through eclipse the PE and K22F is able to run properly.&amp;nbsp; Link to use in searvhing for update in eclipse: "&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://freescale.com/lgfiles/updates/Eclipse/KDS"&gt;http://freescale.com/lgfiles/updates/Eclipse/KDS&lt;/A&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Erich!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 01:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kds-2-0-0-processor-expert-K22FN512LH12-error/m-p/384378#M2180</guid>
      <dc:creator>mjg8t</dc:creator>
      <dc:date>2015-01-04T01:36:29Z</dc:date>
    </item>
  </channel>
</rss>