<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックCan i using C++  in KDS?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-i-using-C-in-KDS/m-p/383458#M2162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When new a project in KDS, we won't need to select C or C++, but the default generate main.c file, is it means KDS only support C project?&lt;/P&gt;&lt;P&gt;The setting of the project properites shows both C and C++ compiler, does it seems support C/C++ mixed programing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Aug 2014 06:58:39 GMT</pubDate>
    <dc:creator>matherinewang</dc:creator>
    <dc:date>2014-08-27T06:58:39Z</dc:date>
    <item>
      <title>Can i using C++  in KDS?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-i-using-C-in-KDS/m-p/383458#M2162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When new a project in KDS, we won't need to select C or C++, but the default generate main.c file, is it means KDS only support C project?&lt;/P&gt;&lt;P&gt;The setting of the project properites shows both C and C++ compiler, does it seems support C/C++ mixed programing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 06:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-i-using-C-in-KDS/m-p/383458#M2162</guid>
      <dc:creator>matherinewang</dc:creator>
      <dc:date>2014-08-27T06:58:39Z</dc:date>
    </item>
    <item>
      <title>Re: Can i using C++  in KDS?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-i-using-C-in-KDS/m-p/383459#M2163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;KDS also supports C++.&lt;/P&gt;&lt;P&gt;The code generated by Processor Expert is always pure C, so the standard main file is also C.&lt;/P&gt;&lt;P&gt;You can replace it by main.cpp if you like.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 14:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-i-using-C-in-KDS/m-p/383459#M2163</guid>
      <dc:creator>georgschmidt</dc:creator>
      <dc:date>2014-08-27T14:09:58Z</dc:date>
    </item>
  </channel>
</rss>