<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Bare bones assembly</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381631#M2090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you want to call the compiler/assembler/linker directly outside Eclipse ?&lt;/P&gt;&lt;P&gt;The tool chain is installed on the folder \KDS_1.1.0\toolchain\bin.&lt;/P&gt;&lt;P&gt;You can call them through a .bat file for instance.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Aug 2014 10:56:10 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-08-28T10:56:10Z</dc:date>
    <item>
      <title>Bare bones assembly</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381630#M2089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way, short of invoking the Gnu assembler and linker directly through command line, of making an assembly-only bare bones KDS project?&amp;nbsp; No startup libraries, no nothing.&amp;nbsp; Older versions of CodeWarrior had an option to do this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 15:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381630#M2089</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-08-26T15:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: Bare bones assembly</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381631#M2090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you want to call the compiler/assembler/linker directly outside Eclipse ?&lt;/P&gt;&lt;P&gt;The tool chain is installed on the folder \KDS_1.1.0\toolchain\bin.&lt;/P&gt;&lt;P&gt;You can call them through a .bat file for instance.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal Irrle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 10:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381631#M2090</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-08-28T10:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: Bare bones assembly</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381632#M2091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, that is not my question.&amp;nbsp; As I said, I know I can invoke the assembler and linker outside of KDS, and I have done that successfully.&amp;nbsp; My question is if there is a way to make a very basic project in KDS that builds a ROM from a single assembly source and still allows you to debug without having to invoke the assembler and linker from a .bat file.&amp;nbsp; Even the most basic KDS project still links in startup libraries, and it creates some C source with a main function.&amp;nbsp; If I take out the C source file, it won't build because it can't find a main function.&amp;nbsp; Code Warrior had the option to do this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 14:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Bare-bones-assembly/m-p/381632#M2091</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-08-28T14:09:23Z</dc:date>
    </item>
  </channel>
</rss>