<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Segger Debug Command File</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-Debug-Command-File/m-p/372553#M1839</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I started to work with KDS using Segger Jlink as Debug interface and I met an issue: I need to launch a command file at the beginning of the debug session to initialize the DDR module of a kinetis K70 because I want to put a section of the code in DDR2, but I do not find where this file can be set.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is possible with Codewarrior: I can provide a .tcl file in the target configuration to initialize the registers of the MCU.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can we do with KDS?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Antonio Cremonini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Nov 2014 10:58:14 GMT</pubDate>
    <dc:creator>acremonini</dc:creator>
    <dc:date>2014-11-26T10:58:14Z</dc:date>
    <item>
      <title>Segger Debug Command File</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-Debug-Command-File/m-p/372553#M1839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I started to work with KDS using Segger Jlink as Debug interface and I met an issue: I need to launch a command file at the beginning of the debug session to initialize the DDR module of a kinetis K70 because I want to put a section of the code in DDR2, but I do not find where this file can be set.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is possible with Codewarrior: I can provide a .tcl file in the target configuration to initialize the registers of the MCU.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can we do with KDS?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Antonio Cremonini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 10:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-Debug-Command-File/m-p/372553#M1839</guid>
      <dc:creator>acremonini</dc:creator>
      <dc:date>2014-11-26T10:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: Segger Debug Command File</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-Debug-Command-File/m-p/372554#M1840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio,&lt;/P&gt;&lt;P&gt;the debugger connection page has several settings you can use, for example the one below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47593i881F92907D4AE636/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can use GDB commands to read/write memory, see as well&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.segger.com/admin/uploads/productDocs/UM08005_JLinkGDBServer.pdf" title="https://www.segger.com/admin/uploads/productDocs/UM08005_JLinkGDBServer.pdf"&gt;https://www.segger.com/admin/uploads/productDocs/UM08005_JLinkGDBServer.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 11:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-Debug-Command-File/m-p/372554#M1840</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-11-26T11:07:05Z</dc:date>
    </item>
  </channel>
</rss>