<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: KDS in CentOS</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308947#M156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, once I realized it's really a 32-bit application, I had no problems copying the entire installation tree from the 64-bit Centos system back to my 32-bit Centos workstation.&amp;nbsp; (I also copied /etc/profile.d/kds.sh, which sets KSDK_PATH even though I can't use KSDK at this time---it doesn't support my chip.)&amp;nbsp; Whoever packaged KDS into the rpm could have made it so that it could load with either 32-bit or 64-bit systems.&amp;nbsp; Oh, well...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now testing beginner-level bare-metal and pex builds on my 32-bit Linux system.&amp;nbsp; So far, so good, but I have a lot to learn.&amp;nbsp; A whole lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Did you hear the one about the guy who fell out of a tenth floor window?&amp;nbsp; As he passed the fifth floor we heard him say, "So far, so good!")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bottom line: My fallback is KDS on the 64-bit Centos installation.&amp;nbsp; If KDS turns out to be unsatisfactory, I can go all the way back to CodeWarrior Special Edition (free) on my Windows workstation.&amp;nbsp; Very clunky; agonizingly slow compared to either of my very modest Linux systems running Kinetis Development Studio.&amp;nbsp; A big hit on productivity.&amp;nbsp; Really big.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Redhat/Centos has become my Linux system of choice for a number of reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jun 2014 23:52:53 GMT</pubDate>
    <dc:creator>davekw7x</dc:creator>
    <dc:date>2014-06-23T23:52:53Z</dc:date>
    <item>
      <title>KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308938#M147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I decided to install KDS RPM version on a fresh Linux VM today and I have a few tips that might help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will need a x64 version of CentOS with 32 bit libraries. I don't think this is a great idea but maybe things have changed since I last looked in to using 32 bit libs on 64 bit.&lt;/P&gt;&lt;P&gt;I followed the answer in this forum post to install the 32 bit libs &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fask.fedoraproject.org%2Fen%2Fquestion%2F9556%2Fhow-do-i-install-32bit-libraries-on-a-64-bit-fedora%2F" rel="nofollow" target="_blank"&gt;https://ask.fedoraproject.org/en/question/9556/how-do-i-install-32bit-libraries-on-a-64-bit-fedora/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You will also need these:&lt;/P&gt;&lt;P&gt;PackageKit-gtk-module.i686&lt;/P&gt;&lt;P&gt;libcanberra-gtk2.i686&lt;/P&gt;&lt;P&gt;gtk2-engines.i686&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FYI: I used the CentOS 6.5 Live DVD with the "Development Tools" package group.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There's probably a better way to do this but it works for me.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Update: KDS also works in Fedora 20 x64 edition. I hope that the GA version will have the dependencies setup so that the package can be installed easier. I wonder if the DEB version of the installer works better.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2014 18:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308938#M147</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2014-05-02T18:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308939#M148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi William,&lt;/P&gt;&lt;P&gt;thanks for sharing!&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 May 2014 07:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308939#M148</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-05-03T07:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308940#M149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded the DEB and had KDS running in Ubuntu 14.04 32 bit edition with much less hassle than the RPM version.&lt;/P&gt;&lt;P&gt;I think the problems with the RPM install will go away once the package and binaries are both 64 bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2014 14:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308940#M149</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2014-05-05T14:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308941#M150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ely,&lt;/P&gt;&lt;P&gt;Yes, agreed. I believe today nearly everyone is using 64bit Linux. I think I should start a survey on this.&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2014 18:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308941#M150</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-05-05T18:50:36Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308942#M151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;New to Freescale and this forum;&amp;nbsp; I just downloaded&lt;EM&gt; kinetis-design-studio-1.0.1-1.i686.rpm&lt;/EM&gt; to install in my Centos 6.5 (32-bit) workstation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With "i686" in the name, it seems to me that it should be a 32-bit distribution.&amp;nbsp; That's the way it's usually done, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alas, when I tried to install, I got the message (among other stuff):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Preparing packages for installation...&lt;/P&gt;&lt;P&gt;D: computing file dispositions&lt;/P&gt;&lt;P&gt;D: opening&amp;nbsp; db index&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /var/lib/rpm/Basenames create mode=0x42&lt;/P&gt;&lt;P&gt;D: 0x00000801&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 21030841&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 15929512 /&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; package kinetis-design-studio-1.0.1-1.x86_64 is intended for a x86_64 architecture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very disappointing!&amp;nbsp; It may be true that "nearly everyone is using 64bit Linux," but I don't use it because of lots of problems with drivers for other tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way that I can get a 32-bit package to install?&amp;nbsp; Any way at all?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bottom line: I am looking to use a chip from KL26 family, and I really like the availability of free, unrestricted Linux tools, but I really don't want to have to make a separate 64-bit Centos installation just for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 16:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308942#M151</guid>
      <dc:creator>davekw7x</dc:creator>
      <dc:date>2014-06-20T16:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308943#M152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dave,&lt;/P&gt;&lt;P&gt;it is a 32bit distribution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 17:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308943#M152</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-06-20T17:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308944#M153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But the package will not install.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hate to repeat myself, but on my 32-bit Centos 6.5 system:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[quote=davekw7x]&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Alas, when I tried to install, I got the message (among other stuff):&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Preparing packages for installation...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;D: computing file dispositions&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;D: opening&amp;nbsp; db index&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /var/lib/rpm/Basenames create mode=0x42&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;D: 0x00000801&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 21030841&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 15929512 /&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; package kinetis-design-studio-1.0.1-1.x86_64 is intended for a x86_64 architecture&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;[/quote]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The package "&lt;EM&gt;is intended for x86_64&lt;/EM&gt;".&amp;nbsp; &lt;EM&gt;x86_64&lt;/EM&gt; is a 64-bit distribution, and rpm refuses to install it on my 32-bit distribution.&amp;nbsp; (But I already said that.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean, if I &lt;EM&gt;have&lt;/EM&gt; to install 64-bit Centos just to run KDS, well, I'll do it (beats the crap out of reviving my Windows machine just for this), but...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 18:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308944#M153</guid>
      <dc:creator>davekw7x</dc:creator>
      <dc:date>2014-06-20T18:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308945#M154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To the Original Poster, William Ely: Thank you for the information.&amp;nbsp; After installing 64-bit Centos 6.5 on a spare workstation and installing the 32-bit libraries that you listed, I was able to install KDS version 1.0.1 and am now ready to explore the wonderful world of Freescale and Kinetis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To Eric Styger:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the thing:&amp;nbsp; The rpm has&amp;nbsp; ".i686" in its name, but the package &lt;EM&gt;inside&lt;/EM&gt; the RPM is for the 64-bit architecture, x86_64.&amp;nbsp; The bottom line is that the rpm is for a 64-bit distribution and won't install on a 32-bit system.&amp;nbsp; Period.&amp;nbsp; Full stop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I note that other vendors (Microchip for example, with MPLABX, Adobe for Acrobat Reader) support builds that work for 32-bit Linux and 64-bit Linux.&amp;nbsp; To run on 64-bit distributions, they need certain 32-bit libraries, as Freescale does for KDS.&amp;nbsp; Why the heck do they (and you) need 32-bit libraries for 64-bit distributions? Well, because there are a number of things about the various 64-bit Linux distributions that just don't work.&amp;nbsp; Maybe it's xorg stuff.&amp;nbsp; Maybe its gtk library stuff.&amp;nbsp; Whatever.&amp;nbsp; Anyhow that's why I have stuck with 32-bit Linux for my main workstations all these years, even though all of my recent platforms have 64-bit CPUs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the KDS team doesn't want to support a 32-bit distribution, that's unfortunate from my perspective, but that's not my call.&amp;nbsp; (It's more than a little annoying, but not fatal.&amp;nbsp; Not yet.&amp;nbsp; I'm still in the preliminary evaluation phase.)&amp;nbsp; If the team can see its way clear to provide a 32-bit package, I'll (gladly) wipe out my 64-bit installation and go back to my main workstation with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the very least, I respectfully suggest that it would be better to name the existing rpm &lt;STRONG&gt; &lt;EM&gt;kinetis-design-studio-1.0.1-1.x86_64&lt;/EM&gt;&lt;/STRONG&gt;&lt;EM&gt;&lt;STRONG&gt;.&lt;/STRONG&gt;&lt;STRONG&gt;rpm&lt;/STRONG&gt;&lt;/EM&gt; or some such thing so that people with some experience in "normal" ways of doing things won't waste their time (and board bandwidth) trying to make things happen according to convention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Dave&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 15:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308945#M154</guid>
      <dc:creator>davekw7x</dc:creator>
      <dc:date>2014-06-21T15:12:30Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308946#M155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Glad that I could help.&lt;/P&gt;&lt;P&gt;I have not had time to play around with KDS since my original post. I intend to keep my CodeWarrior subscription for another year so KDS will have some time to mature before I migrate over to it.&lt;/P&gt;&lt;P&gt;If you are serious about using 32 bit only then you might want to try Ubuntu. I had a much easier time getting KDS installed on Ubuntu than an RPM based distribution. I didn't do any testing with it other than making sure that the application opened though.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 21:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308946#M155</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2014-06-23T21:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: KDS in CentOS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308947#M156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, once I realized it's really a 32-bit application, I had no problems copying the entire installation tree from the 64-bit Centos system back to my 32-bit Centos workstation.&amp;nbsp; (I also copied /etc/profile.d/kds.sh, which sets KSDK_PATH even though I can't use KSDK at this time---it doesn't support my chip.)&amp;nbsp; Whoever packaged KDS into the rpm could have made it so that it could load with either 32-bit or 64-bit systems.&amp;nbsp; Oh, well...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now testing beginner-level bare-metal and pex builds on my 32-bit Linux system.&amp;nbsp; So far, so good, but I have a lot to learn.&amp;nbsp; A whole lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Did you hear the one about the guy who fell out of a tenth floor window?&amp;nbsp; As he passed the fifth floor we heard him say, "So far, so good!")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bottom line: My fallback is KDS on the 64-bit Centos installation.&amp;nbsp; If KDS turns out to be unsatisfactory, I can go all the way back to CodeWarrior Special Edition (free) on my Windows workstation.&amp;nbsp; Very clunky; agonizingly slow compared to either of my very modest Linux systems running Kinetis Development Studio.&amp;nbsp; A big hit on productivity.&amp;nbsp; Really big.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Redhat/Centos has become my Linux system of choice for a number of reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 23:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-in-CentOS/m-p/308947#M156</guid>
      <dc:creator>davekw7x</dc:creator>
      <dc:date>2014-06-23T23:52:53Z</dc:date>
    </item>
  </channel>
</rss>