<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KDS UI enhancement request in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351229#M1361</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for checking.  Yes, I have two monitors and yes, it is usually not an issue if I spread KDS across both monitors or split the windows, or double click on the tab to maximize the window.  Unfortunately I also have to look at other windows along with KDS.  I guess I will just have to get 4 monitors! LOL!  Or maybe an 8k monitor! &lt;A href="http://www.pcgamesn.com/both-nvidia-and-amd-are-preparing-for-8k-for-the-human-eye-that-resolution-is-close-to-perfection" target="test_blank"&gt;http://www.pcgamesn.com/both-nvidia-and-amd-are-preparing-for-8k-for-the-human-eye-that-resolution-is-close-to-perfection&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Oct 2014 12:01:54 GMT</pubDate>
    <dc:creator>johnbaker</dc:creator>
    <dc:date>2014-10-27T12:01:54Z</dc:date>
    <item>
      <title>KDS UI enhancement request</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351226#M1358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is the little things that make a big difference! ;-)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let's say I have 20 files open in KDS and am looking at one of them.&amp;nbsp; I then need to open another file to look at.&amp;nbsp; As soon as I open another file, the TAB of the one I was just looking at disappears and I have to click on the arrow &lt;STRONG&gt;way-y-y-y-y-y&lt;/STRONG&gt; to the right of the screen to find it again. I would have thought that it would hide the TAB of the oldest looked at file?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to make the tabs FIFO&amp;nbsp; instead of LIFO?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John Baker&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 20:17:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351226#M1358</guid>
      <dc:creator>johnbaker</dc:creator>
      <dc:date>2014-10-24T20:17:16Z</dc:date>
    </item>
    <item>
      <title>Re: KDS UI enhancement request</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351227#M1359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not aware of any settings to change this, and I doubt there is one. It is the way how it is in Eclipse.&lt;/P&gt;&lt;P&gt;One tip I have is that you can double click on the tab of the file to enlarge everything: that probably will reduce the chance that tabs are hidden as you have more screen real estate.&lt;/P&gt;&lt;P&gt;If you have multiple monitors, then you can have a second main window or the source files on a separate monitor, see &lt;A href="http://mcuoneclipse.com/2012/02/29/go-multiply-and-detach-multiple-screens-with-eclipse/" title="http://mcuoneclipse.com/2012/02/29/go-multiply-and-detach-multiple-screens-with-eclipse/"&gt;Go, multiply and detach: Multiple Screens with Eclipse | MCU on Eclipse&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;You can use CTRL+F6 (see &lt;A href="http://mcuoneclipse.com/2012/07/20/switching-source-files-in-the-eclipse-editor-ctrltab/" title="http://mcuoneclipse.com/2012/07/20/switching-source-files-in-the-eclipse-editor-ctrltab/"&gt;Switching Source Files in the Eclipse Editor (CTRL+TAB) | MCU on Eclipse&lt;/A&gt;) to switch between the source files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Oct 2014 06:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351227#M1359</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-10-25T06:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: KDS UI enhancement request</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351228#M1360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know if this description is off any use:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The Editor view is populated with editor panels in the order they are opened. So this is FIFO based on when they are opened (maybe you mean last accessed order).&lt;/LI&gt;&lt;LI&gt;When a particular editor is selected then the IDE 'intelligently' displays the tab for the selected editor.&amp;nbsp; By intelligently I mean that it doesn't change the tabs displayed unless it has to. &lt;/LI&gt;&lt;LI&gt;It never re-orders the tabs.&lt;/LI&gt;&lt;LI&gt;If you have a large number of tabs open then the visible tabs will change to those that are near to the one selected.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Given the above I find it useful to re-order the tabs into related items e.g. the header file next to the corresponding source file or files that represent a locus if interest.&amp;nbsp; This helps to keep the tabs of useful files visible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another thing that may also help is the navigation buttons &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47037i5327D31554B05EE1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; that allow you to move between several areas of interest.&lt;/P&gt;&lt;P&gt;It is also possible to have multiple Editor views visible at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For what it is worth I would vote for the current behaviour :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Oct 2014 00:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351228#M1360</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-10-26T00:54:43Z</dc:date>
    </item>
    <item>
      <title>Re: KDS UI enhancement request</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351229#M1361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for checking.  Yes, I have two monitors and yes, it is usually not an issue if I spread KDS across both monitors or split the windows, or double click on the tab to maximize the window.  Unfortunately I also have to look at other windows along with KDS.  I guess I will just have to get 4 monitors! LOL!  Or maybe an 8k monitor! &lt;A href="http://www.pcgamesn.com/both-nvidia-and-amd-are-preparing-for-8k-for-the-human-eye-that-resolution-is-close-to-perfection" target="test_blank"&gt;http://www.pcgamesn.com/both-nvidia-and-amd-are-preparing-for-8k-for-the-human-eye-that-resolution-is-close-to-perfection&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 12:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351229#M1361</guid>
      <dc:creator>johnbaker</dc:creator>
      <dc:date>2014-10-27T12:01:54Z</dc:date>
    </item>
    <item>
      <title>Re: KDS UI enhancement request</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351230#M1362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, that was very useful knowledge.  I did not realize this until I just now played with it.  The tab pages are in a listview control that corresponds to the drop down selector at the end of the tabs.  If I select the last item it pushes the view to the end and I do not see the first tabs.  Likewise when I select the first tab the view shifts back to the beginning and I no longer see the end tabs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the info,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John Baker&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 12:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-UI-enhancement-request/m-p/351230#M1362</guid>
      <dc:creator>johnbaker</dc:creator>
      <dc:date>2014-10-27T12:24:06Z</dc:date>
    </item>
  </channel>
</rss>