<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Is there a &amp;quot;timer macro&amp;quot;?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349824#M1297</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You will need to configure a hardware timer. It's the best way to get an accurate time based clock on an embedded board. You need a hardware timer to drive the clocking software. The PE clock functions are returning 0 because they haven't been connected to a hardware timer. In processor expert you will have to configure a hardware timer and connect it to the clock software driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the K64 you have several options to generate a clock/timer. There is the Systick interrupt in the base ARM core registers, there's the PITs (Peripheral interrupt timers)&amp;nbsp; and the previously mentioned RTC (Real Time clock). The real time clock can be battery backed up and can keep time when the device is powered down. You will have to pick a timer peripheral based on the timers accuracy and when it needs to run.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Dec 2014 14:36:41 GMT</pubDate>
    <dc:creator>ndavies</dc:creator>
    <dc:date>2014-12-15T14:36:41Z</dc:date>
    <item>
      <title>Is there a "timer macro"?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349821#M1294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I need a (hopefully) simple timer. BUT I'd prefer not to use an hardware timer.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I explain. I need to measure if a time interval elapsed. My ideal piece of code will be something that gives me the clock ticks since the power on and then divides them by the clock frequency.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In plain old C I'd write&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;clock_t tmr = clock();&lt;/P&gt;&lt;P&gt;... Operation&lt;/P&gt;&lt;P&gt;int elapsed_ms = (clock()- tmr*1000)*/CLOCKS_PER_SEC;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But... In Kinetis Design Studio (Processor Expert project, so no C++, and no RTOS) the "clock" function returns always 0 and CLOCKS_PER_SEC is equal to 100.&lt;/P&gt;&lt;P&gt;Do you know if there is something I can use? As already stated I'd prefer not to use some hardware timers, because this is just a part of the program and I'd like to limit interferences with other parts.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW... I'm using a FRDM-K64F board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Dec 2014 13:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349821#M1294</guid>
      <dc:creator>frarugi87</dc:creator>
      <dc:date>2014-12-14T13:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a "timer macro"?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349822#M1295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Franceesco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have never used KSD, but I think you can use RTC. If you want not to use RTC, you can make a software timer by using RTC Time Seconds interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Dec 2014 19:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349822#M1295</guid>
      <dc:creator>yasuhikokoumoto</dc:creator>
      <dc:date>2014-12-14T19:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a "timer macro"?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349823#M1296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;What do you mean by "RTC"? Is there a software component called RTC or yuo mean an external or internal piece of hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I wrote, I could use a timer to generate interrupts or to track time in another way, but I'd prefer not to use other peripherals...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 14:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349823#M1296</guid>
      <dc:creator>frarugi87</dc:creator>
      <dc:date>2014-12-15T14:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a "timer macro"?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349824#M1297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You will need to configure a hardware timer. It's the best way to get an accurate time based clock on an embedded board. You need a hardware timer to drive the clocking software. The PE clock functions are returning 0 because they haven't been connected to a hardware timer. In processor expert you will have to configure a hardware timer and connect it to the clock software driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the K64 you have several options to generate a clock/timer. There is the Systick interrupt in the base ARM core registers, there's the PITs (Peripheral interrupt timers)&amp;nbsp; and the previously mentioned RTC (Real Time clock). The real time clock can be battery backed up and can keep time when the device is powered down. You will have to pick a timer peripheral based on the timers accuracy and when it needs to run.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 14:36:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349824#M1297</guid>
      <dc:creator>ndavies</dc:creator>
      <dc:date>2014-12-15T14:36:41Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a "timer macro"?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349825#M1298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Francesco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I mean the internal hardware module by RTC (Real Time Clock). RTC is a timer which is not reset under any resets other than power on. It can cause an alarm interrupt, an overflow interrupt and a time seconds interrupt. The time seconds interrupt is an interrupt by every second. The RTC is used to hold elapsed time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2014 20:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-there-a-quot-timer-macro-quot/m-p/349825#M1298</guid>
      <dc:creator>yasuhikokoumoto</dc:creator>
      <dc:date>2014-12-15T20:57:37Z</dc:date>
    </item>
  </channel>
</rss>