<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Generate .bin file from KDS 3.2</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256661#M10188</link>
    <description>&lt;P&gt;I guess either your bootloader has a problem or your application has a problem.&lt;/P&gt;&lt;P&gt;If you just look at the bin file you won't see the problem.&lt;/P&gt;&lt;P&gt;You have to kick in the debugger to see what is going on: See for example &lt;A href="https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Mon, 05 Apr 2021 11:22:22 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2021-04-05T11:22:22Z</dc:date>
    <item>
      <title>Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514351#M6777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's possible to generate the .bin file when running 'Build project' in a SDK_2.0 project?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To avoid having to do it manually.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;arm-none-eabi-objcopy -O binary hello_world_frdmk64f.elf hello_world_frdmk64f.bin&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 18:17:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514351#M6777</guid>
      <dc:creator>javierhernande1</dc:creator>
      <dc:date>2016-06-03T18:17:48Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514352#M6778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;see &lt;A href="https://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/" title="https://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/"&gt;https://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 18:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514352#M6778</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-06-03T18:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514353#M6779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Works as a charm. Very useful articles, thanks very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 19:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/514353#M6779</guid>
      <dc:creator>javierhernande1</dc:creator>
      <dc:date>2016-06-03T19:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256597#M10185</link>
      <description>&lt;P&gt;My main program starts at 0x5000 so my linker file is&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;MEMORY {
  m_interrupts (RX) : ORIGIN = 0x00005000, LENGTH = 0x000001E8
  m_text      (RX) : ORIGIN = 0x00005410, LENGTH = 0x000FABF0
  m_data      (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
  m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
  /*m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010*/
}&lt;/LI-CODE&gt;&lt;P&gt;But a bin file generated at the offset 0x5000 not at 0. Even if I feed the file to a bootloader starting at 0x5000 in the bin file - main program doesn't run after exit from a bootloader.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 08:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256597#M10185</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2021-04-05T08:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256608#M10186</link>
      <description>&lt;P&gt;That's exepcted, see &lt;A href="https://sourceware.org/binutils/docs/binutils/objcopy.html" target="_blank" rel="noopener"&gt;https://sourceware.org/binutils/docs/binutils/objcopy.html&lt;/A&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;objcopy can be used to generate a raw binary file by using an output target of ‘binary’ (e.g., use -O binary). When objcopy generates a raw binary file, it will essentially produce a memory dump of the contents of the input object file. All symbols and relocation information will be discarded. The memory dump will start at the load address of the lowest section copied into the output file.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If you indeed want to have a binary starting with address 0, then I recommend using the SRecord tool which allows you to do any kind of manipulation and conversion, see for example &lt;A href="https://mcuoneclipse.com/2018/03/07/converting-binary-files-to-intel-hex-format-with-the-srecord-tool/" target="_blank" rel="noopener"&gt;https://mcuoneclipse.com/2018/03/07/converting-binary-files-to-intel-hex-format-with-the-srecord-tool/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 08:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256608#M10186</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-04-05T08:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256621#M10187</link>
      <description>&lt;P&gt;Thank you. I did so. But when I burn the file with a bootloader - the main program doesn't&amp;nbsp; run. May be I miss something?&lt;/P&gt;&lt;P&gt;I cut out the block 0-4fff that bootloader address space and burn the file starting at 0x5000.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 09:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256621#M10187</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2021-04-05T09:34:45Z</dc:date>
    </item>
    <item>
      <title>Re: Generate .bin file from KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256661#M10188</link>
      <description>&lt;P&gt;I guess either your bootloader has a problem or your application has a problem.&lt;/P&gt;&lt;P&gt;If you just look at the bin file you won't see the problem.&lt;/P&gt;&lt;P&gt;You have to kick in the debugger to see what is going on: See for example &lt;A href="https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Mon, 05 Apr 2021 11:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Generate-bin-file-from-KDS-3-2/m-p/1256661#M10188</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-04-05T11:22:22Z</dc:date>
    </item>
  </channel>
</rss>