<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Build Issue on Windows 10</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1235011#M10173</link>
    <description>&lt;P&gt;Thank you for the reply Erich.&amp;nbsp; However, that did not fix the issue (tried multiple times).&lt;/P&gt;&lt;P&gt;However, I did seem to fix the issue.&amp;nbsp; I had a hunch that the IDE couldn't find the compiler/linker, so I looked at the build settings.&amp;nbsp; The compiler/linker works if I switch the Builder Type from External builder to Internal builder.&amp;nbsp; The output of the console looks radically different from my home computer setup, but it does work properly.&amp;nbsp; I will try to figure out why External works on my home computer...&lt;/P&gt;&lt;P&gt;- Rick&lt;/P&gt;</description>
    <pubDate>Tue, 23 Feb 2021 13:15:38 GMT</pubDate>
    <dc:creator>rppolicy</dc:creator>
    <dc:date>2021-02-23T13:15:38Z</dc:date>
    <item>
      <title>Build Issue on Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1234603#M10171</link>
      <description>&lt;P&gt;I recently had a PC refresh at work and Kinetis Design Studio V3.2 does not work on it.&amp;nbsp; The new PC is windows 10, but my home computer is also windows 10 and has no issues.&lt;/P&gt;&lt;P&gt;Using a New Processor Expert project (pretty much blank), I get the following error:&lt;/P&gt;&lt;P&gt;Static_Code/System/subdir.mk:24: recipe for target 'Static_Code/System/CPU_Init.o' failed&lt;BR /&gt;make: *** [Static_Code/System/CPU_Init.o] Error 244&lt;/P&gt;&lt;P&gt;I imported a known good project and get the exact same error.&amp;nbsp; Installing KDS 3.2 twice did not fix the issue.&lt;/P&gt;&lt;P&gt;Does anyone know what the issue could be?&lt;/P&gt;&lt;P&gt;- Rick&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 22:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1234603#M10171</guid>
      <dc:creator>rppolicy</dc:creator>
      <dc:date>2021-02-22T22:47:13Z</dc:date>
    </item>
    <item>
      <title>Re: Build Issue on Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1234929#M10172</link>
      <description>&lt;P&gt;Hi Rick,&lt;/P&gt;&lt;P&gt;- try a Project &amp;gt; Clean, then a build&lt;/P&gt;&lt;P&gt;- or: delete the output (Debug) folder first.&lt;/P&gt;&lt;P&gt;I guess you have an invalid make file somehow in the build output folder&lt;/P&gt;&lt;P&gt;Otherwise: can you post your project?&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 10:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1234929#M10172</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-02-23T10:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: Build Issue on Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1235011#M10173</link>
      <description>&lt;P&gt;Thank you for the reply Erich.&amp;nbsp; However, that did not fix the issue (tried multiple times).&lt;/P&gt;&lt;P&gt;However, I did seem to fix the issue.&amp;nbsp; I had a hunch that the IDE couldn't find the compiler/linker, so I looked at the build settings.&amp;nbsp; The compiler/linker works if I switch the Builder Type from External builder to Internal builder.&amp;nbsp; The output of the console looks radically different from my home computer setup, but it does work properly.&amp;nbsp; I will try to figure out why External works on my home computer...&lt;/P&gt;&lt;P&gt;- Rick&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 13:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Build-Issue-on-Windows-10/m-p/1235011#M10173</guid>
      <dc:creator>rppolicy</dc:creator>
      <dc:date>2021-02-23T13:15:38Z</dc:date>
    </item>
  </channel>
</rss>