<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Preferred development system for FRDM-KE02Z?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030723#M10105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've recently got hold of a FRDM-KE02Z board (MKE02Z64VQH2) but I am struggling to get KDS set up to work with it. None of the SDKs 1.0.0-1.3.0 seem to support this board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the recommended development environment? I have access to OS X, Linux and Windows 10 hosts in order of preference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 00:27:12 GMT</pubDate>
    <dc:creator>qu1j0t3</dc:creator>
    <dc:date>2019-12-11T00:27:12Z</dc:date>
    <item>
      <title>Preferred development system for FRDM-KE02Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030723#M10105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've recently got hold of a FRDM-KE02Z board (MKE02Z64VQH2) but I am struggling to get KDS set up to work with it. None of the SDKs 1.0.0-1.3.0 seem to support this board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the recommended development environment? I have access to OS X, Linux and Windows 10 hosts in order of preference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 00:27:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030723#M10105</guid>
      <dc:creator>qu1j0t3</dc:creator>
      <dc:date>2019-12-11T00:27:12Z</dc:date>
    </item>
    <item>
      <title>Re: Preferred development system for FRDM-KE02Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030724#M10106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Toby,&lt;/P&gt;&lt;P&gt;Yes, MKE02Z64VQH2 is an old product. It will not be supported by any SDK. You can use KDS or Codewarrior. In KDS, you can only create project by processor expert.&lt;/P&gt;&lt;P&gt;I recommend MKE02Z64VQH4. It's price is almost same as MKE02Z64VQH2. It has most update 2.6 version SDK. And you can use MCUXpresso.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 09:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030724#M10106</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-12-11T09:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: Preferred development system for FRDM-KE02Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030725#M10107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thankyou, that was good advice. I got the board working with Processor Expert.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also updated the firmware to Segger OpenSDA v1. I had to do that update with Windows XP in VirtualBox, as Windows 10 caused bootloader errors, and OS X couldn't do the update either. After that update I can use the board from OS X and debug in KDS 3.2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 14:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030725#M10107</guid>
      <dc:creator>qu1j0t3</dc:creator>
      <dc:date>2019-12-12T14:22:49Z</dc:date>
    </item>
    <item>
      <title>Re: Preferred development system for FRDM-KE02Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030726#M10108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently started using MKE02z64VQH4 in MCUXpresso IDE with 2.6 version SDK. However, to my horror, discovered that even the simple timer library functions in file "fsl_ftm.c" are causing hardware faults during initialisation calls to "FTM_Init(FTM_BASEADDR, &amp;amp;ftmInfo)" whenever trying to initialise FTM0 and FTM1 modules. The library works only with FTM2 module. Hardware faults seem to be caused by access violations to certain registers viz. Mode,&amp;nbsp;SYNC etc. which appear to have not been implemented in FTM0/FTM1 modules. However, processor reference manual does not indicate clearly about implementation of these registers. At my wits end as to what is going on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 08:36:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Preferred-development-system-for-FRDM-KE02Z/m-p/1030726#M10108</guid>
      <dc:creator>skaval99</dc:creator>
      <dc:date>2020-03-26T08:36:21Z</dc:date>
    </item>
  </channel>
</rss>