<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR K60N512 Toggling Pin for probing in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Toggling-Pin-for-probing/m-p/275510#M9849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K60 procut GPIO pin toggle speed should match with your requirement (toggle &amp;gt; 0.01ms).&lt;/P&gt;&lt;P&gt;There are many timer resource for customer to use.&lt;/P&gt;&lt;P&gt;Customer can use a PIT generate period interrupt and toggle the GPIO pin in PIT interrupt service routine.&lt;/P&gt;&lt;P&gt;Customer also could use FlexTimer module to generate PWM signal.&lt;/P&gt;&lt;P&gt;I attached some example code for your reference.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jun 2013 02:13:34 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2013-06-05T02:13:34Z</dc:date>
    <item>
      <title>TWR K60N512 Toggling Pin for probing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Toggling-Pin-for-probing/m-p/275509#M9848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I want to toggle a pin very fast from the CPU to a TP or a point on the elevation board, which pin shall I choose?&lt;/P&gt;&lt;P&gt;The pin shall be toggled in my main loop &amp;gt; 0.01 ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following thread suggest using FTM or GPIO.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/117330"&gt;Re: Timers of less than 1 ms&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the correct configuration for using the FTM1_CH0:&lt;/P&gt;&lt;P&gt;k60 ref man (12.2.14)&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;SIM-&amp;gt;SCGC6&lt;/TD&gt;&lt;TD&gt;|= SIM_SCGC6_FTM1_MASK; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the k60 ref manual and SCH, FTM has several alternatives (10.3.1). &lt;/P&gt;&lt;P&gt;CPU: TRACED2\FTM1_CH0 K8 PTA8 ALT3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 23:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Toggling-Pin-for-probing/m-p/275509#M9848</guid>
      <dc:creator>mrandreas</dc:creator>
      <dc:date>2013-06-04T23:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: TWR K60N512 Toggling Pin for probing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Toggling-Pin-for-probing/m-p/275510#M9849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K60 procut GPIO pin toggle speed should match with your requirement (toggle &amp;gt; 0.01ms).&lt;/P&gt;&lt;P&gt;There are many timer resource for customer to use.&lt;/P&gt;&lt;P&gt;Customer can use a PIT generate period interrupt and toggle the GPIO pin in PIT interrupt service routine.&lt;/P&gt;&lt;P&gt;Customer also could use FlexTimer module to generate PWM signal.&lt;/P&gt;&lt;P&gt;I attached some example code for your reference.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 02:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Toggling-Pin-for-probing/m-p/275510#M9849</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-06-05T02:13:34Z</dc:date>
    </item>
  </channel>
</rss>