<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic entering and exiting low power-modes in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275356#M9834</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do i have to set MCG settings again after exiting VLPR mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;before going into VLPR, MCG is set to BLPI . in VLPR i run some Calculations, UART communications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;further i want to put the processor to VLLS1 mode and wake up the processor from reset flow to VLPR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how do i do it ? having problemsin waking up processor from VLLS1 with LLWU interrupts&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jun 2013 10:06:34 GMT</pubDate>
    <dc:creator>pradyumnakammar</dc:creator>
    <dc:date>2013-06-05T10:06:34Z</dc:date>
    <item>
      <title>entering and exiting low power-modes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275356#M9834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do i have to set MCG settings again after exiting VLPR mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;before going into VLPR, MCG is set to BLPI . in VLPR i run some Calculations, UART communications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;further i want to put the processor to VLLS1 mode and wake up the processor from reset flow to VLPR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how do i do it ? having problemsin waking up processor from VLLS1 with LLWU interrupts&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 10:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275356#M9834</guid>
      <dc:creator>pradyumnakammar</dc:creator>
      <dc:date>2013-06-05T10:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: entering and exiting low power-modes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275357#M9835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kammardi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you need to set it back. For all lower power mode, you can reference this link &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL2&amp;amp;nodeId=01624698C9E3EC&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL2&amp;amp;nodeId=01624698C9E3EC&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;, in item "Simulation and Models-BSDL". After you installing, you can find demo code in path ...\KL05-SC\klxx-sc-baremetal\build\iar\low_power_demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Pau;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 03:54:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275357#M9835</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-06-06T03:54:50Z</dc:date>
    </item>
    <item>
      <title>Re: entering and exiting low power-modes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275358#M9836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes i have already seen this example!! &lt;/P&gt;&lt;P&gt;in the example they exit VLPR through reset not with ant exiting routine!! with the help of the document AN4503 which the Freescale has provided i have written the exiting routine but still LLWU does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;things i have done and tried :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. RUN mode (FEE) --&amp;gt; VLLS1 wakes to RUN for LLWU pin and module interrupt through reset-flow &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. RUN (FEE) --&amp;gt; VLPR(BLPE) for comunication --&amp;gt; Exit VLPR routine --&amp;gt; VLLS1 . Now LLWU interrupt does not work but RTC interrupt works&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tried the workaround in eratta still LLWU not working (e5472)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 08:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/entering-and-exiting-low-power-modes/m-p/275358#M9836</guid>
      <dc:creator>pradyumnakammar</dc:creator>
      <dc:date>2013-06-06T08:26:05Z</dc:date>
    </item>
  </channel>
</rss>