<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: PROBLEM FREESCALE CUP</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274908#M9659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Edoardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does your battery provides enough power to move the TFC-Motor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer to this site and keep me informed if this helped you: &lt;A href="https://community.nxp.com/docs/DOC-1284"&gt;The Freescale Cup Knowledge Center&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;B.R.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hector Sanchez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jan 2014 15:23:33 GMT</pubDate>
    <dc:creator>hectorsanchez</dc:creator>
    <dc:date>2014-01-06T15:23:33Z</dc:date>
    <item>
      <title>PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274907#M9658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i'm new here and my name is Edoardo.&lt;/P&gt;&lt;P&gt;For the Freescale Cup i'm using a FRDM-KL25Z and a TFC-Motor Shield.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i attach the board to the shield and get power on the shield with the battery the Board not turn on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How i can solve this problem ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help Me !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Dec 2013 14:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274907#M9658</guid>
      <dc:creator>edoardocavallot</dc:creator>
      <dc:date>2013-12-22T14:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274908#M9659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Edoardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does your battery provides enough power to move the TFC-Motor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer to this site and keep me informed if this helped you: &lt;A href="https://community.nxp.com/docs/DOC-1284"&gt;The Freescale Cup Knowledge Center&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;B.R.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hector Sanchez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 15:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274908#M9659</guid>
      <dc:creator>hectorsanchez</dc:creator>
      <dc:date>2014-01-06T15:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274909#M9660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the battery is ok.&lt;/P&gt;&lt;P&gt;if the shield is powered by the battery, the board doesn't work. It work only by the USB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2014 08:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274909#M9660</guid>
      <dc:creator>edoardocavallot</dc:creator>
      <dc:date>2014-01-17T08:20:49Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274910#M9661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Edoardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have had some problems with power on the FRDM KL25 boards on revision E, because there are some changes on power circuits between revisions D and E. Looking at the shield schematic, it can be seen that battery voltage is present at the "+V_BATTERY" node, which is connected to pin 16 of J9 of the FRDM board. This pin is the "P5_9V_VIN" access point for the FRDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look at the FRDM revD schematic, you will see that this node is connected to the input of a 3.3V regulator. The 5V power from both USB connectors also go to this point through blocking diodes, so an external battery will shut off 5V power from USBs. If your board is revD, the 7.2V from the batteries tould be directly transformed to 3.3V on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, if you check on revE schematic, you will notice that there is a diode between this connection point and the voltage regulator. I suppose that you may have a problem with this diode, which is D10. I suggest powering the shield board alone with the battery and checking if you find 7.2V on the shield pin 16 of J9 (use pin 14 or 12 of the same connector as reference). If you find the full voltage, connect the battery directly between pins 16 ( + ) and 14 or 12 ( - ) of J9 on FRDM board. If the board does not power up, you may have a problem with D10. In that case, you could substitute this diode, although it is a SMD component. You may also short its terminals, and I believe you would not have any problem with that since D11 and D12 still protect your circuit from problems with connecting both battery and USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2014 16:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274910#M9661</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2014-01-17T16:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274911#M9662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio,&lt;/P&gt;&lt;P&gt;i solve it. Now the car work perfectly :smileycheck:&lt;/P&gt;&lt;P&gt;Thanks for your suggestions :smileyhappy:&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Antonio Quevedo ha scritto:&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Hello Edoardo,&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;I have had some problems with power on the FRDM KL25 boards on revision E, because there are some changes on power circuits between revisions D and E. Looking at the shield schematic, it can be seen that battery voltage is present at the "+V_BATTERY" node, which is connected to pin 16 of J9 of the FRDM board. This pin is the "P5_9V_VIN" access point for the FRDM.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;If you look at the FRDM revD schematic, you will see that this node is connected to the input of a 3.3V regulator. The 5V power from both USB connectors also go to this point through blocking diodes, so an external battery will shut off 5V power from USBs. If your board is revD, the 7.2V from the batteries tould be directly transformed to 3.3V on the board.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Now, if you check on revE schematic, you will notice that there is a diode between this connection point and the voltage regulator. I suppose that you may have a problem with this diode, which is D10. I suggest powering the shield board alone with the battery and checking if you find 7.2V on the shield pin 16 of J9 (use pin 14 or 12 of the same connector as reference). If you find the full voltage, connect the battery directly between pins 16 ( + ) and 14 or 12 ( - ) of J9 on FRDM board. If the board does not power up, you may have a problem with D10. In that case, you could substitute this diode, although it is a SMD component. You may also short its terminals, and I believe you would not have any problem with that since D11 and D12 still protect your circuit from problems with connecting both battery and USB.&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;I hope it helps&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Cheers&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;Antonio&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thanks for all,&lt;/P&gt;&lt;P&gt;Edoardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2014 12:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274911#M9662</guid>
      <dc:creator>edoardocavallot</dc:creator>
      <dc:date>2014-01-20T12:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: PROBLEM FREESCALE CUP</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274912#M9663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That would be interesting if you could give details on how you solved it. What data did you get from the power lines?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Antonio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2014 12:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PROBLEM-FREESCALE-CUP/m-p/274912#M9663</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2014-01-20T12:36:49Z</dc:date>
    </item>
  </channel>
</rss>