<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Driver software for MK20DX256VLH7 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274832#M9654</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a driver package for the following chip? MK20DX256VLH7 For example like the STM32F4 DSP and standard peripherals library?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Dec 2013 22:43:23 GMT</pubDate>
    <dc:creator>tcmichals</dc:creator>
    <dc:date>2013-12-21T22:43:23Z</dc:date>
    <item>
      <title>Driver software for MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274832#M9654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a driver package for the following chip? MK20DX256VLH7 For example like the STM32F4 DSP and standard peripherals library?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Dec 2013 22:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274832#M9654</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2013-12-21T22:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Driver software for MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274833#M9655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&lt;/P&gt;&lt;P&gt;FSL has only a peripherals library for KE02 now. However I think our demo code is useful for reference and it's easily to use. Please refer to it for details.&lt;/P&gt;&lt;P&gt;The link of TWR-K20D72 is post as below. Wish hope.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/32bit/software/KINETIS_72MHz_SRC.zip?WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Downloads&amp;amp;Parent_nodeId=1331244528573714554979&amp;amp;Parent_pageType=product" title="http://www.freescale.com/files/32bit/software/KINETIS_72MHz_SRC.zip?WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Downloads&amp;amp;Parent_nodeId=1331244528573714554979&amp;amp;Parent_pageType=product"&gt;http://www.freescale.com/files/32bit/software/KINETIS_72MHz_SRC.zip?WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESC…&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 03:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274833#M9655</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2013-12-24T03:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: Driver software for MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274834#M9656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is helpful.&amp;nbsp; Guess there is only two options use the codewarrior or go off and create a code branch.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 17:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274834#M9656</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2013-12-24T17:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Driver software for MK20DX256VLH7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274835#M9657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&lt;/P&gt;&lt;P&gt;There's the third way to crate your project quickly.&amp;nbsp; When you download the the demo code and install it, you'll find a make_new_project.exe in ........\KINETIS_72MHz_SRC\KINETIS_72MHz_SRC\build\iar, then simply double-click this icon and a command prompt pop-up window will prompt you for a project name, copy the helloworld project and rename all of the necessary files for your new project to work correctly.This method is&lt;/P&gt;&lt;P&gt;more quickly and convinence than you use IDE software create a project directly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41420iC1C54AE0721C8F11/image-size/large?v=v2&amp;amp;px=999" title="4.jpg" alt="4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Dec 2013 02:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-software-for-MK20DX256VLH7/m-p/274835#M9657</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2013-12-25T02:18:34Z</dc:date>
    </item>
  </channel>
</rss>