<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K10 Internal Clock Reference in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274821#M9652</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The use of the clock source will depend upon the tolerance in stability of clock that you are looking at. You can use the internal clock in your application if it meets your tolerance over the specified range of temperature your application is going to work in. Details on the clock tolerance/variance you can get in the electrical specifications of the MCG clocks in the device datasheet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the clock configuration you will have to use the FEI mode and you will have to use the 32.768Khz internal RC. You cannot use the 4Mhz for this mode as that clock cannot be connected to the FLL module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will use the 4Mhz internal in VLPW and VPLR modes. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It will be a good idea to go through the chapter on MCG in the documentation &lt;A href="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1" title="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1"&gt;http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This explains all the modes in detail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cheers !!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Feb 2013 05:05:23 GMT</pubDate>
    <dc:creator>deepakrana</dc:creator>
    <dc:date>2013-02-27T05:05:23Z</dc:date>
    <item>
      <title>K10 Internal Clock Reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274820#M9651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MK10DX series micro controller. I want to use Internal Clock reference (either 32.768KHz or 4MHZ) to achieve 72MHz core frequency.&lt;/P&gt;&lt;P&gt;1. Is it recommended to use internal clock reference for generating such high core clock (72MHz)?&lt;/P&gt;&lt;P&gt;2. If using Internal clock reference is recommended then which mode should I use (FEI or FBI) if I want to use Fast Internal Clock Reference (4MHz)&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2013 16:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274820#M9651</guid>
      <dc:creator>deelipomana</dc:creator>
      <dc:date>2013-02-26T16:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: K10 Internal Clock Reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274821#M9652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The use of the clock source will depend upon the tolerance in stability of clock that you are looking at. You can use the internal clock in your application if it meets your tolerance over the specified range of temperature your application is going to work in. Details on the clock tolerance/variance you can get in the electrical specifications of the MCG clocks in the device datasheet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the clock configuration you will have to use the FEI mode and you will have to use the 32.768Khz internal RC. You cannot use the 4Mhz for this mode as that clock cannot be connected to the FLL module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will use the 4Mhz internal in VLPW and VPLR modes. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It will be a good idea to go through the chapter on MCG in the documentation &lt;A href="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1" title="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1"&gt;http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This explains all the modes in detail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cheers !!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2013 05:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274821#M9652</guid>
      <dc:creator>deepakrana</dc:creator>
      <dc:date>2013-02-27T05:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: K10 Internal Clock Reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274822#M9653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Deelip, how is the project going?&lt;/P&gt;&lt;P&gt;Keep us posted! :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2013 20:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-Internal-Clock-Reference/m-p/274822#M9653</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-03-05T20:08:12Z</dc:date>
    </item>
  </channel>
</rss>