<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FTM doesn't work in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-doesn-t-work/m-p/274118#M9566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody.&lt;/P&gt;&lt;P&gt;I'm trying to configure a simple two channels CPWM on FTM0 using MKE02Z32VLD, but I can't. I've tried several ways but no one works. It happens that all register are configured, but FTM0_C0V and FTM0_C1V are set equal to 0. So one channel is always at 100% and one is at 0%, because of the ES1A and ES1B settings. I've tried to write to this registers in several ways but the result is always the same. I don't know why. Pins are redirect in a correct way so I can see FTM0_CH0 and FTM0_CH1 on pin 32 and 33. Clock is gated... Any other suggestion?&lt;/P&gt;&lt;P&gt;Thanks a lot to everybody!&lt;/P&gt;&lt;P&gt;Roberto&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41012i09618AA1D7347A04/image-size/large?v=v2&amp;amp;px=999" title="FTM.jpg" alt="FTM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Mar 2014 12:26:17 GMT</pubDate>
    <dc:creator>robertogiovinet</dc:creator>
    <dc:date>2014-03-04T12:26:17Z</dc:date>
    <item>
      <title>FTM doesn't work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-doesn-t-work/m-p/274118#M9566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody.&lt;/P&gt;&lt;P&gt;I'm trying to configure a simple two channels CPWM on FTM0 using MKE02Z32VLD, but I can't. I've tried several ways but no one works. It happens that all register are configured, but FTM0_C0V and FTM0_C1V are set equal to 0. So one channel is always at 100% and one is at 0%, because of the ES1A and ES1B settings. I've tried to write to this registers in several ways but the result is always the same. I don't know why. Pins are redirect in a correct way so I can see FTM0_CH0 and FTM0_CH1 on pin 32 and 33. Clock is gated... Any other suggestion?&lt;/P&gt;&lt;P&gt;Thanks a lot to everybody!&lt;/P&gt;&lt;P&gt;Roberto&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41012i09618AA1D7347A04/image-size/large?v=v2&amp;amp;px=999" title="FTM.jpg" alt="FTM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 12:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-doesn-t-work/m-p/274118#M9566</guid>
      <dc:creator>robertogiovinet</dc:creator>
      <dc:date>2014-03-04T12:26:17Z</dc:date>
    </item>
    <item>
      <title>Re: FTM doesn't work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-doesn-t-work/m-p/274119#M9567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everybody&lt;/P&gt;&lt;P&gt;I found how to make it works fine. Below the text to configure CPWM on FTM0 channels. Is mandatary the order to set registers, and wite a value (for example 0) in FTM0_CNT register.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43001i37ED7E55A394320C/image-size/large?v=v2&amp;amp;px=999" title="FTM.jpg" alt="FTM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this can help.&lt;/P&gt;&lt;P&gt;Roberto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Mar 2014 15:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-doesn-t-work/m-p/274119#M9567</guid>
      <dc:creator>robertogiovinet</dc:creator>
      <dc:date>2014-03-05T15:36:57Z</dc:date>
    </item>
  </channel>
</rss>