<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiprocessor Kinetis in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273610#M9520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your support. During my DSP benchmark tests i also used an STM32F407 for comparison, and i found that the STM32 was loosing cycles when executing from RAM. It has some 1-cycle RAM, but cannot execute from that range of memory. So a 2 processor&amp;nbsp; K10 77 MHz system is cheaper and more powerful than a 180 MHz STM32, i mean as integer DSP. And the new STM32 parts with TDM I2S are not available yet.&lt;/P&gt;&lt;P&gt;Another question: Do the 100, 120 and 150 MHz Kinetis variants all execute from 1-cycle RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 17:10:47 GMT</pubDate>
    <dc:creator>dieterteuchert</dc:creator>
    <dc:date>2013-06-13T17:10:47Z</dc:date>
    <item>
      <title>Multiprocessor Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273608#M9518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While i have made good progress on implementing and optimizing DSP procedures for Cortex M4, i was wondering if there was ready to use support for multiprocessor solutions, for example a debugger that works with an oldfashioned JTAG chain including two or four MK10 processors and which could be used to initialize flash on such a board. As far as i remember, the main problem with FPGA embedded multiprocessor solutions was debugging them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 11:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273608#M9518</guid>
      <dc:creator>dieterteuchert</dc:creator>
      <dc:date>2013-06-04T11:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: Multiprocessor Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273609#M9519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis product supports JTAG chain. Customer can select to use Segger J-Link tool or UNLINK2 debugger tool to control the chain.&lt;/P&gt;&lt;P&gt;More detailed info, please check below link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.segger.com/admin/uploads/productDocs/UM08001_JLinkARM.pdf" style="text-indent: 0px;"&gt;http://www.segger.com/admin/uploads/productDocs/UM08001_JLinkARM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;amp; &lt;A href="http://www.keil.com/support/man/docs/ulink2/ulink2_su_chaining.htm" style="text-indent: 0px;"&gt;http://www.keil.com/support/man/docs/ulink2/ulink2_su_chaining.htm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There also need to do some modification with debug interface, please check attached file as a reference.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 02:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273609#M9519</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-06-05T02:40:14Z</dc:date>
    </item>
    <item>
      <title>Re: Multiprocessor Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273610#M9520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your support. During my DSP benchmark tests i also used an STM32F407 for comparison, and i found that the STM32 was loosing cycles when executing from RAM. It has some 1-cycle RAM, but cannot execute from that range of memory. So a 2 processor&amp;nbsp; K10 77 MHz system is cheaper and more powerful than a 180 MHz STM32, i mean as integer DSP. And the new STM32 parts with TDM I2S are not available yet.&lt;/P&gt;&lt;P&gt;Another question: Do the 100, 120 and 150 MHz Kinetis variants all execute from 1-cycle RAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 17:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273610#M9520</guid>
      <dc:creator>dieterteuchert</dc:creator>
      <dc:date>2013-06-13T17:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: Multiprocessor Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273611#M9521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Yes, Kinetis 100MHz, 120/150MHz products all with 1-cycle access SRAM.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 04:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiprocessor-Kinetis/m-p/273611#M9521</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-06-14T04:25:39Z</dc:date>
    </item>
  </channel>
</rss>