<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックProblem programming srec on FRDM board, additional question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-programming-srec-on-FRDM-board-additional-question/m-p/270951#M9188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, followed Eric's suggestion on how to create a s19 file which turns out to be a *.hex file.&amp;nbsp; When I drop the file onto the MSD drive&lt;/P&gt;&lt;P&gt;nothing happens.&amp;nbsp; My application is trying to use the console function or printf out CDC to Tera Term.&amp;nbsp; It works in the normal manner when using the debugger&lt;/P&gt;&lt;P&gt;agent and such, but thought this would be a cool path for customers who need a special demo and don't want to mess with code compilation.&amp;nbsp; Is this beyond the scope of the MSD bootloader capabilities?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The file starts like this:&lt;/P&gt;&lt;P&gt;S0140000766973696F6E346C65676163792E68657837&lt;/P&gt;&lt;P&gt;S113000000300020FD060000F1080000FD0800009B&lt;/P&gt;&lt;P&gt;S1130010FD080000FD080000FD080000FD080000C8&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Apr 2013 03:27:29 GMT</pubDate>
    <dc:creator>steve_fae</dc:creator>
    <dc:date>2013-04-17T03:27:29Z</dc:date>
    <item>
      <title>Problem programming srec on FRDM board, additional question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-programming-srec-on-FRDM-board-additional-question/m-p/270951#M9188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, followed Eric's suggestion on how to create a s19 file which turns out to be a *.hex file.&amp;nbsp; When I drop the file onto the MSD drive&lt;/P&gt;&lt;P&gt;nothing happens.&amp;nbsp; My application is trying to use the console function or printf out CDC to Tera Term.&amp;nbsp; It works in the normal manner when using the debugger&lt;/P&gt;&lt;P&gt;agent and such, but thought this would be a cool path for customers who need a special demo and don't want to mess with code compilation.&amp;nbsp; Is this beyond the scope of the MSD bootloader capabilities?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The file starts like this:&lt;/P&gt;&lt;P&gt;S0140000766973696F6E346C65676163792E68657837&lt;/P&gt;&lt;P&gt;S113000000300020FD060000F1080000FD0800009B&lt;/P&gt;&lt;P&gt;S1130010FD080000FD080000FD080000FD080000C8&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 03:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-programming-srec-on-FRDM-board-additional-question/m-p/270951#M9188</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-04-17T03:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Problem programming srec on FRDM board, additional question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-programming-srec-on-FRDM-board-additional-question/m-p/270952#M9189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you try to use the DOS/cmd shell 'copy' command instead of using the Windows Explorer (press Windows+r, then enter the command 'cmd', then use the 'copy' command to copy the file to the bootloader).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 05:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-programming-srec-on-FRDM-board-additional-question/m-p/270952#M9189</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-04-17T05:40:17Z</dc:date>
    </item>
  </channel>
</rss>