<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flexbus initialization and test for external SRAM..? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270863#M9180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, there is also a similar problem on my device. We have added 512 KB external SRAM to our K60n512 board. The initialization function is the same as described above (as the code from Todd) or in AN4393, except the following&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set FlexBus Base address for CS0.&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSAR = 0x70000000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set CS control register for CS0. Addr s&amp;amp;h, 4 WS, AutoAck, 8bit port.&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSCR = FB_CSCR_ASET(1) | FB_CSCR_RDAH(1) | FB_CSCR_WS(4) |&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FB_CSCR_AA_MASK | FB_CSCR_PS(1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set FlexBus Base address mask for CS0 and set valid (enable).&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSMR = FB_CSMR_BAM(0x07) | FB_CSMR_V_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When checking FB_CS0 in the oscilloscope while doing some read/write at base address, no signals can be observed from FB_CS0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be appreciated if anyone could provide some possible hints or information about this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Mar 2013 00:33:50 GMT</pubDate>
    <dc:creator>logancheng</dc:creator>
    <dc:date>2013-03-11T00:33:50Z</dc:date>
    <item>
      <title>Re: Flexbus initialization and test for external SRAM..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270863#M9180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, there is also a similar problem on my device. We have added 512 KB external SRAM to our K60n512 board. The initialization function is the same as described above (as the code from Todd) or in AN4393, except the following&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set FlexBus Base address for CS0.&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSAR = 0x70000000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set CS control register for CS0. Addr s&amp;amp;h, 4 WS, AutoAck, 8bit port.&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSCR = FB_CSCR_ASET(1) | FB_CSCR_RDAH(1) | FB_CSCR_WS(4) |&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FB_CSCR_AA_MASK | FB_CSCR_PS(1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Set FlexBus Base address mask for CS0 and set valid (enable).&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSMR = FB_CSMR_BAM(0x07) | FB_CSMR_V_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When checking FB_CS0 in the oscilloscope while doing some read/write at base address, no signals can be observed from FB_CS0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be appreciated if anyone could provide some possible hints or information about this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2013 00:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270863#M9180</guid>
      <dc:creator>logancheng</dc:creator>
      <dc:date>2013-03-11T00:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus initialization and test for external SRAM..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270864#M9181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I check the Flexbu setting code without any problem.&lt;/P&gt;&lt;P&gt;AN4393 the Flexbus initialization code with below Flexbus clock frequency drivid setting:&lt;/P&gt;&lt;P&gt;SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided&lt;/P&gt;&lt;P&gt;Please make sure the Flexbus clock frequency not exceed 50MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 06:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270864#M9181</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-04-17T06:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus initialization and test for external SRAM..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270865#M9182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I know, the flexbus of K60 mapped at the following addresses:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119280i3930FC2059905070/image-size/large?v=v2&amp;amp;px=999" title="11.png" alt="11.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;None of them starts from 0x70000000, so would you please try to change &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;FB-&amp;gt;CS[0].CSAR to 0x60000000 or 0x90000000 and try again?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly let me know if the problem is still there.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2013 07:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270865#M9182</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-04-18T07:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus initialization and test for external SRAM..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270866#M9183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is solved, CS0 signal can be observed now. After much effort in trying and also checking with hardware designer, we found out it was the following two points that caused the problem:&lt;/P&gt;&lt;P&gt;1. hardware: the address line connection was incorrect on board&lt;/P&gt;&lt;P&gt;2. software:&amp;nbsp; the base address used during read/write was not correctly written, it should be&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define MRAM_START_ADDRESS (*(vuint8*)(0x70000000))&lt;/P&gt;&lt;P&gt;FB_CSAR0 = (uint32)&amp;amp;MRAM_START_ADDRESS;&lt;/P&gt;&lt;P&gt;and when accessing&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;*(vuint8*)(&amp;amp;MRAM_START_ADDRESS + n) = wdata8;&lt;/P&gt;&lt;P&gt;rdata8=0x00; //clear data variable;&lt;/P&gt;&lt;P&gt;rdata8=(*(vuint8*)(&amp;amp;MRAM_START_ADDRESS + n));&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, many thanks for your reply!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2013 00:29:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-Flexbus-initialization-and-test-for-external-SRAM/m-p/270866#M9183</guid>
      <dc:creator>logancheng</dc:creator>
      <dc:date>2013-04-19T00:29:26Z</dc:date>
    </item>
  </channel>
</rss>