<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Doubt about KwikStik j-link usage...</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164816#M905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;BLOCKQUOTE&gt;Ethernet Help wrote:&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;On the kwikstick schematic there is a signal named:&amp;nbsp;JTAG_EZB_CS_b﻿&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not familiar with this signal.. should i connect it or not? If yes how?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;As far as I can tell, that's not used by the J-Link.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But note that due to a design error, you can't debug external processors without a circuit change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is that with the ON/OFF switch in the OFF position, the K40 is not powered. Which isn't a problem for the JTAG lines, as they're 5-V tolerant and so don't interfere when the K40 is not powered.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the RESET line is protected by an internal diode to the K40's VCC line.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So you can't pull RESET high with the on-board J-LINK without adding a diode in series with the K40's RESET line (anode to K40 pin 74, and remove R113 (there is an internal pullup on /RESET in the K40).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As they say, "if it hasn't been tested, it doesn't work".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Oct 2011 03:53:34 GMT</pubDate>
    <dc:creator>bikenomad</dc:creator>
    <dc:date>2011-10-27T03:53:34Z</dc:date>
    <item>
      <title>Doubt about KwikStik j-link usage...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164815#M904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i want to use the KwikStik j-link to program an externa Kinetis. What circuit should i add to create a proper connection? I was looking at the kwikstik schematic, and the signals that are connected to the header, are connected directly to the onboard kinetis..&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the kwikstick schematic there is a signal named:&amp;nbsp;JTAG_EZB_CS_b﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not familiar with this signal.. should i connect it or not? If yes how?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2011 04:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164815#M904</guid>
      <dc:creator>EthernetHelp</dc:creator>
      <dc:date>2011-09-06T04:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: Doubt about KwikStik j-link usage...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164816#M905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;BLOCKQUOTE&gt;Ethernet Help wrote:&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;On the kwikstick schematic there is a signal named:&amp;nbsp;JTAG_EZB_CS_b﻿&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not familiar with this signal.. should i connect it or not? If yes how?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;As far as I can tell, that's not used by the J-Link.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But note that due to a design error, you can't debug external processors without a circuit change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is that with the ON/OFF switch in the OFF position, the K40 is not powered. Which isn't a problem for the JTAG lines, as they're 5-V tolerant and so don't interfere when the K40 is not powered.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the RESET line is protected by an internal diode to the K40's VCC line.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So you can't pull RESET high with the on-board J-LINK without adding a diode in series with the K40's RESET line (anode to K40 pin 74, and remove R113 (there is an internal pullup on /RESET in the K40).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As they say, "if it hasn't been tested, it doesn't work".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 03:53:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164816#M905</guid>
      <dc:creator>bikenomad</dc:creator>
      <dc:date>2011-10-27T03:53:34Z</dc:date>
    </item>
    <item>
      <title>Re: Doubt about KwikStik j-link usage...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164817#M906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you bikenomad, I disconnected power supply according to errata documentation (chipbead F5) and I disconnected RESET line temporally (I don't have diode small enough&amp;nbsp;to fit between pin and via at the moment). It is working now. I've tried it with TWR K60 external target.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 17:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Doubt-about-KwikStik-j-link-usage/m-p/164817#M906</guid>
      <dc:creator>Mr_Honey</dc:creator>
      <dc:date>2011-11-01T17:09:16Z</dc:date>
    </item>
  </channel>
</rss>