<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KE02 pinout in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268406#M8887</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am laying out a prototype board for the MKE02Z64VQH2 (64 pin package).&amp;nbsp; I want to use both SPIs, but the reference manual seems to have an error.&amp;nbsp; SPI0_MOSI is shown on pin 31 and 59. SPI0_SCK is shown on pins 32 and 60.&amp;nbsp; I do not see a SPI1_SCK, SPI1_MOSI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas of the correct pinout?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Aug 2013 15:53:02 GMT</pubDate>
    <dc:creator>dporada</dc:creator>
    <dc:date>2013-08-21T15:53:02Z</dc:date>
    <item>
      <title>KE02 pinout</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268406#M8887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am laying out a prototype board for the MKE02Z64VQH2 (64 pin package).&amp;nbsp; I want to use both SPIs, but the reference manual seems to have an error.&amp;nbsp; SPI0_MOSI is shown on pin 31 and 59. SPI0_SCK is shown on pins 32 and 60.&amp;nbsp; I do not see a SPI1_SCK, SPI1_MOSI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas of the correct pinout?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 15:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268406#M8887</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2013-08-21T15:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: KE02 pinout</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268407#M8888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Donald,&lt;/P&gt;&lt;P&gt;&amp;nbsp; In the &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/MKE02P64M20SF0.pdf"&gt;datasheet&lt;/A&gt; on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 19:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268407#M8888</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-08-21T19:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: KE02 pinout</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268408#M8889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oops, you are correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was looking at Alt 2 where the rest of the SPI pins were configured, not at Alt 3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don Porada&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 20:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE02-pinout/m-p/268408#M8889</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2013-08-21T20:04:20Z</dc:date>
    </item>
  </channel>
</rss>