<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMPU: Freescale vs. ARM core</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MPU-Freescale-vs-ARM-core/m-p/267571#M8829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working on a project which uses a Kinetis K70&amp;nbsp; processor and I found that according to the data sheets there are two MPU (memory protection unit). One added by Freescale, one placed in the Cortex-M4 core.&lt;/P&gt;&lt;P&gt;Did anyone used them in the past and is able to answer a few questions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both MPU's at the same time? Which means is it possible to define some sections in the code MPU and some in the outer (Freescale) MPU?&lt;/P&gt;&lt;P&gt;And if it possible are there any correlations or priorities between them? Like the core MPU wins over the outer MPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Aug 2013 08:27:46 GMT</pubDate>
    <dc:creator>thomasgrieger</dc:creator>
    <dc:date>2013-08-21T08:27:46Z</dc:date>
    <item>
      <title>MPU: Freescale vs. ARM core</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MPU-Freescale-vs-ARM-core/m-p/267571#M8829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working on a project which uses a Kinetis K70&amp;nbsp; processor and I found that according to the data sheets there are two MPU (memory protection unit). One added by Freescale, one placed in the Cortex-M4 core.&lt;/P&gt;&lt;P&gt;Did anyone used them in the past and is able to answer a few questions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both MPU's at the same time? Which means is it possible to define some sections in the code MPU and some in the outer (Freescale) MPU?&lt;/P&gt;&lt;P&gt;And if it possible are there any correlations or priorities between them? Like the core MPU wins over the outer MPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 08:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MPU-Freescale-vs-ARM-core/m-p/267571#M8829</guid>
      <dc:creator>thomasgrieger</dc:creator>
      <dc:date>2013-08-21T08:27:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPU: Freescale vs. ARM core</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MPU-Freescale-vs-ARM-core/m-p/267572#M8830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The Cortex-M4 MPU is an option ARM offers, however it was not used on Kinetis. Instead we only use the Freescale one since it provides a lot more features like non-core master awareness. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 19:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MPU-Freescale-vs-ARM-core/m-p/267572#M8830</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2013-08-21T19:29:31Z</dc:date>
    </item>
  </channel>
</rss>