<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MQX RTOS for FRDM_K20D50M</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267036#M8742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, MQX will work on the K20 at 50Mhz. But as the harware is not the same, the bsp has to be modified, but many things can be reused. Have a look at this threat for BSP porting. You have the 'Clone' tool in the /tools MQX folder, you can start cloning the TWR-K20D50 BSP and make the modifications for the FRDM board. Internal peripherals drivers will be the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/306640"&gt;https://community.freescale.com/thread/306640&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And yes, you can debug using OPENSDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jul 2013 13:29:29 GMT</pubDate>
    <dc:creator>LuisCasado</dc:creator>
    <dc:date>2013-07-11T13:29:29Z</dc:date>
    <item>
      <title>MQX RTOS for FRDM_K20D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267035#M8741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;I try using MQX RTOS to programing microcontroller from FRDM_K20D50M board (MK20DX128). I found information that TWR_K20D50M is fully supported by MQX. Does anybody know if FRDM-K20D50M board can cooperate witch full MQX RTOS to? Can I use OPENSDA to debug? Anyone tried it? &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 12:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267035#M8741</guid>
      <dc:creator>madagaskar</dc:creator>
      <dc:date>2013-07-11T12:17:27Z</dc:date>
    </item>
    <item>
      <title>Re: MQX RTOS for FRDM_K20D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267036#M8742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, MQX will work on the K20 at 50Mhz. But as the harware is not the same, the bsp has to be modified, but many things can be reused. Have a look at this threat for BSP porting. You have the 'Clone' tool in the /tools MQX folder, you can start cloning the TWR-K20D50 BSP and make the modifications for the FRDM board. Internal peripherals drivers will be the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/306640"&gt;https://community.freescale.com/thread/306640&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And yes, you can debug using OPENSDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 13:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267036#M8742</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2013-07-11T13:29:29Z</dc:date>
    </item>
    <item>
      <title>Re: MQX RTOS for FRDM_K20D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267037#M8743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel,&lt;/P&gt;&lt;P&gt;Luis is correct.&lt;/P&gt;&lt;P&gt;A general rule of thumb is Freedom boards are supported with MQXLite and Tower boards with MQX.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 18:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-RTOS-for-FRDM-K20D50M/m-p/267037#M8743</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-07-11T18:55:07Z</dc:date>
    </item>
  </channel>
</rss>