<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Using FlexTimer Module with Kinetis K70...</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266710#M8712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much Jing, that's exactly what I was looking for, but I had a problem using this component because it seems to get stuck in its "init" function (FTM_Init()), so I debugged this function and found that after writting or reading to/from FTMx_SC register, the code jumps to the "Unhandled int code" of the debugger (in Cpu.c) which is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PE_ISR(Cpu_Interrupt)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* This code can be changed using the CPU component property "Build Options / Unhandled int code" */&lt;/P&gt;&lt;P&gt;&amp;nbsp; PE_DEBUGHALT();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so I tried to disable it as indicated in comments but nothing changed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know what is going on? because is the first time I work with freescale and its environment.&lt;/P&gt;&lt;P&gt;Also, I don't know either if this component should replace the PWM_LDD because only has the "init" method, so how can I control the PWM in runtime?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Juan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2013 12:43:41 GMT</pubDate>
    <dc:creator>juannava</dc:creator>
    <dc:date>2013-12-18T12:43:41Z</dc:date>
    <item>
      <title>Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266708#M8710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with the TWR-K70F120M and Processor Expert, trying to generate a PWM signal in Complementary Mode with Dead-Time insertion but I don't see how to do it in PE, it just let me use two channels (n and n+1) independently but not in Combine Mode, so I modified (manually) the generated file (PWM.c) as indicated in the reference manual, but it doesn't work anyway. Does anyone know how to configure the FTM to operate in this mode?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 15:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266708#M8710</guid>
      <dc:creator>juannava</dc:creator>
      <dc:date>2013-12-17T15:37:37Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266709#M8711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juan Nava,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use the init_FTM component, in this component, you can set up the combine mode and dead-time like following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39953i81AE136A160CF639/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; you can try it now!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I wish it helps you!&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 02:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266709#M8711</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2013-12-18T02:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266710#M8712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much Jing, that's exactly what I was looking for, but I had a problem using this component because it seems to get stuck in its "init" function (FTM_Init()), so I debugged this function and found that after writting or reading to/from FTMx_SC register, the code jumps to the "Unhandled int code" of the debugger (in Cpu.c) which is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PE_ISR(Cpu_Interrupt)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* This code can be changed using the CPU component property "Build Options / Unhandled int code" */&lt;/P&gt;&lt;P&gt;&amp;nbsp; PE_DEBUGHALT();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so I tried to disable it as indicated in comments but nothing changed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know what is going on? because is the first time I work with freescale and its environment.&lt;/P&gt;&lt;P&gt;Also, I don't know either if this component should replace the PWM_LDD because only has the "init" method, so how can I control the PWM in runtime?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Juan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 12:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266710#M8712</guid>
      <dc:creator>juannava</dc:creator>
      <dc:date>2013-12-18T12:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266711#M8713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juan Nava,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I will create a project on the basis of your expect as soon as possible, and give you for your reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please wait patiently! Thank you !&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 03:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266711#M8713</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2013-12-19T03:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266712#M8714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I create a project, and test it ok, it use the Init_FTM component, and configure the FTM0_CH0 and FTM0_CH1 in combine mode, make the deadtime to about 10us.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please find my project in the attachments, it is based on the TWR-K70F120M.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The test result as follows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; Picture1&lt;/STRONG&gt;:with no deadtime&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40310iB664C495D3243707/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; Picture2&lt;/STRONG&gt;:with about 10 us deadtime&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40693i111FC3036351A48F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish my answer helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact with me!&lt;/P&gt;&lt;P&gt;Thank you and best regards!&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 06:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266712#M8714</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2013-12-19T06:37:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266713#M8715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing, thank you very much for the example, it is very useful.&lt;/P&gt;&lt;P&gt;I greatly appreciate your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Juan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2013 12:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266713#M8715</guid>
      <dc:creator>juannava</dc:creator>
      <dc:date>2013-12-19T12:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: Using FlexTimer Module with Kinetis K70...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266714#M8716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; No thanks, you are welcome!&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 01:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FlexTimer-Module-with-Kinetis-K70/m-p/266714#M8716</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2013-12-20T01:07:31Z</dc:date>
    </item>
  </channel>
</rss>