<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-KL25Z and P5V_USB in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-and-P5V-USB/m-p/266103#M8600</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I had the same issue using 'normal' shields which do need that 5V from the CPU board. The current FRDM board does not generate/provide that 5V.&lt;/P&gt;&lt;P&gt;As long as you get exactly that 5V through VIN, I do not see an issue connecting VIN with the 5V pin. What I'm using with my boards is &lt;A href="http://www.pololu.com/catalog/product/2119"&gt;S7V7F5&lt;/A&gt; DC-DC step up/down voltage converter board from Pololu which generates 5V from 2.7..11.8V. Ideal for battery voltage coming from VIN. See &lt;A href="http://mcuoneclipse.com/2013/02/08/zumo-line-following-with-frdm-kl25z/" title="http://mcuoneclipse.com/2013/02/08/zumo-line-following-with-frdm-kl25z/"&gt;Zumo Line Following with FRDM-KL25Z &lt;/A&gt;for details. I use the same concept for other shields.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2013 07:41:43 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2013-02-21T07:41:43Z</dc:date>
    <item>
      <title>FRDM-KL25Z and P5V_USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-and-P5V-USB/m-p/266102#M8599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been working with the Freedom board for some time now. Recently I was asked to develop a demo using this board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My demo is making use of a couple of Arduino shield and in order for viewers to better see what exactly is being used I have had a larger breakout board built, whereby I can unstack the boards and lay them all out, side-by-side. I am powering up the Freedom board via J9-20 (5V-9VIN). One of my shields is expecting 5V on J9-10 (5V_USB). Looking at the available documentation it is apparent that J9-10 gets voltage off of either the USB_SDA or USB_KL25Z connectors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my question, provided my shield can accomodate 5-9V, which it can, are there any issues with my simply tying J9-10 to J9-20? From what I see J9-10 does not seem to be connected to much of anything on the Freedom board, aside from the Shottky diodes, off P5V_SDA and P5V_KL25Z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Cameron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2013 18:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-and-P5V-USB/m-p/266102#M8599</guid>
      <dc:creator>chaegle</dc:creator>
      <dc:date>2013-02-20T18:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z and P5V_USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-and-P5V-USB/m-p/266103#M8600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I had the same issue using 'normal' shields which do need that 5V from the CPU board. The current FRDM board does not generate/provide that 5V.&lt;/P&gt;&lt;P&gt;As long as you get exactly that 5V through VIN, I do not see an issue connecting VIN with the 5V pin. What I'm using with my boards is &lt;A href="http://www.pololu.com/catalog/product/2119"&gt;S7V7F5&lt;/A&gt; DC-DC step up/down voltage converter board from Pololu which generates 5V from 2.7..11.8V. Ideal for battery voltage coming from VIN. See &lt;A href="http://mcuoneclipse.com/2013/02/08/zumo-line-following-with-frdm-kl25z/" title="http://mcuoneclipse.com/2013/02/08/zumo-line-following-with-frdm-kl25z/"&gt;Zumo Line Following with FRDM-KL25Z &lt;/A&gt;for details. I use the same concept for other shields.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 07:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-and-P5V-USB/m-p/266103#M8600</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-02-21T07:41:43Z</dc:date>
    </item>
  </channel>
</rss>