<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: New Kinetis Flash SWAP mechanism</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163897#M856</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dave and Earl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coincidentally I added the Flash Swap mechanism as an option to the uTasker serial loader today. Although I am not fully convinced yet, there may be some cases where the swap could be of interest (mainly swapping between two installed versions and also using applications that don't need to be linked to a boot loader address).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this thread you can find more details as well as operating code (that is, real loader/application and not just an example of a dummy swap):&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/587268"&gt;Re: Development of Swap in FRDM_K64&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;P.S. The subject of boot loaders comes up time and time again and it is quite frustrating to see hundered of companies porting and redeveloping effectively the same solution (often derivatives of AN2295, AN4764, AN4379, AN4368, or Kboot) - it must cost the industry millions in man power costs to re-develop the same wheel so often and to port examples from one processor to another or from one IDE to another.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Don't forget that the uTasker serial loader does all of these, for almost all Kinetis parts/families and all standard IDEs. It even allows mixing them. if you can't decide whether a USB-MSD device is what you need or a USB-MSD host (memory stick) you can simply enable both and allow the board to automatcially detect the mode it should use - or mix with Kboot at the same time - or even enable the old developer's serial loader (AN2295) on a UART, just for the hell of it...Complete flexibility - no porting - completely validated and proven solutions. And now with Swap Block support too ...;-)&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Nov 2015 04:48:00 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-11-13T04:48:00Z</dc:date>
    <item>
      <title>New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163871#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to work with the 'new' FLASH-controller-based Flash-block SWAP mechanism, as described in the new section 28.4.12.14 in Rev 5 of the Family Reference Manual (I am working with the 144-pin K60, as it happens).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Firstly, while this section may be a decent description of the chip functions, it is rather poor at describing how one would best USE this functionality to implement a reliable system update process.&amp;nbsp; For instance, table 28-67 details a number of combinations of 'fault' the system as a whole must contend with, but I THINK it is sufficient to test MGSTAT0 for '0' and a State Code of '1' to indicate a 'non fault' condition coming out of reset -- anything else means something happened along the way.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One thing that is NOT defined in ANY reasonable way I can discern is the use of the 'Flash Address' in each command.&amp;nbsp; It sort of reads like this is some kind of 'password' that is set by the initialize command and must match in all other commands, BUT I set this to a non-random 0xA530 pattern, and NOW my IAR debug-download (thru Segger Jlink 4.34a tools) complains that it can't erase the sector starting at 0xA000, and I can no longer download code!&amp;nbsp;(Although it appears to me that all 496K from 0x4000 to 0x7FFFF is erased.)&amp;nbsp;So, one question is, is there any way to return this SWAP state machine to the uninitialized state so I can get my chip working again???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In any case, my issues might stem from a deeper issue relative to how this swap mechanism is designed to work, as opposed to how I WANT to use it.&amp;nbsp;&amp;nbsp;The previous swap mechanism (a battery-backed bit in the RTC section) did nothing more or less than fully swap the 256K flash blocks.&amp;nbsp; SO, how I HAD been using 'swap' functions was as a 'safety catch' mechanism to reliably update the bootloader.&amp;nbsp; That is, I have the first 16K block (minimum FPROT register protection size), as contains the reset vector, dedicated to bootloader space.&amp;nbsp; The remaining 496K is all application space which the bootloader can update, in our case from external SPI memory downloaded previously (two total images there for necessary protection from a fatally flawed update).&amp;nbsp; So, the SWAP function would come in when I need to update the actual bootloader itself as part of some major system change.&amp;nbsp; For that, what I HAD been doing is to:&lt;/P&gt;&lt;P&gt;1 - copy the current bootloader out to 0x40000 (start of second 256K).&lt;/P&gt;&lt;P&gt;2 - if that works, set the 'swap' bit so that from this point ANY reset will restart the original bootloader&lt;/P&gt;&lt;P&gt;3 - erase the first 16K and load in the new bootloader image.&lt;/P&gt;&lt;P&gt;4 - if that all goes well (CRC passes) then clear the 'swap' bit and hit reset to run the new code.&lt;/P&gt;&lt;P&gt;5 - for ANY failure, including a reset while the banks are swapped, indicates a need to restore the original bootloader&lt;/P&gt;&lt;P&gt;This way the system is almost ALWAYS running the banks in 'normal' 0/1 order.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Firstly, I don't see that I can use the new 'swap' function for just this 'backup' function as I was doing -- the diagram clearly indicates a need for 'resets' and erase operations in each bank to move around the states.&amp;nbsp; But I do have a fundamental concern here as well -- while this mechanism is discussed as a SWAP process, the descriptions talk mostly of which bank is 'active' (at address 0) as if the 'other bank' were somehow not 'fully normally accessible' at the 256K address.&amp;nbsp; Can I still get my full 496K application space with this new SWAP initialized?&amp;nbsp; Or is this whole operation geared directly at applications that have two 256K 'application spaces' that one would ping-pong between?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Earl Goodrich II&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 02:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163871#M830</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2011-08-31T02:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163872#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no way to recover the original state if you enabled swap feature once.&lt;/P&gt;&lt;P&gt;It means that "Erase all" command will be disabled and you cannot use Jtag debugger to flash it anymore...&lt;/P&gt;&lt;P&gt;We haven't tried EzPort yet. It might be an alternative way to get the chip flashed when swap feature have been executed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To touch with swap feature, you should start with a downloader to write data from external media to 2nd flash block , confirm that it works fine before enable swap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should have 3-5 boards/chips on you hand before playing with this &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 05:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163872#M831</guid>
      <dc:creator>Dekiru</dc:creator>
      <dc:date>2011-08-31T05:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163873#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the tidbits!&amp;nbsp; I have been doing some more experimentation and I now have a better understanding of the Flash Address supplied in each command -- we actually have to dedicate&amp;nbsp;that area of USER flash memory in BOTH banks that will contain the one flag word that tracks the stages of update for each bank, AND is used at reset to evaluate said results -- which is to say that word MUST be dedicated, which at the very least breaks the 'contiguous flash addressing' of 'user space' if (like me!) you are trying to use MOST of the flash for one application-image.&amp;nbsp; It certainly looks like any attempt to use this new SWAP feature for anything other than true ping-pong (256K max application!) will be extremely complicated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I see what you mean about JTAG tools!&amp;nbsp; The 'implicit protection' of the WHOLE SECTOR containing at LEAST the 'active bank' flag word, and ALSO that in&amp;nbsp;the 'other bank' if it's not set into 'update mode', certainly prevents a 'debug' tool access to one or two whole 2K sectors, further complicating any attempt to use this feature.&amp;nbsp; I can't understand why these 'flag words' couldn't have been stored 'somewhere else' to stay out of our way!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And this seems to be yet another irreversible flash process that lets programmers and tools create permanently broken assemblies!&amp;nbsp; I truly don't understand the lack of at least JTAG-capable erase-recovery modes...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Earl Goodrich II&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 09:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163873#M832</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2011-08-31T09:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163874#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kinetis silicon Rev1.4 change the swap flash mechanism:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;﻿﻿&lt;/P&gt;&lt;P&gt;&lt;U&gt;Kinetis (100MHz devices)&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Rev 1.0 – old swap method&lt;/P&gt;&lt;P&gt;Rev 1.1 – new swap method - more robust to power loss&lt;/P&gt;&lt;DIV class="O1"&gt;•&amp;nbsp; When swap system is initialized Erase-All-Blocks is disabled&lt;/DIV&gt;&lt;DIV class="O1"&gt;•&amp;nbsp; Swap system cannot go back to uninitialized&lt;/DIV&gt;&lt;P&gt;Rev 1.2&lt;/P&gt;&lt;DIV class="O1"&gt;•&amp;nbsp; Same as rev 1.1 except slight change to initialization&lt;/DIV&gt;&lt;P&gt;Rev 1.4 – swap enhancement&lt;/P&gt;&lt;DIV class="O1"&gt;• Erase-All-Blocks is not disabled when swap is initialized&lt;/DIV&gt;&lt;DIV class="O1"&gt;• Swap system can be set back to uninitialized&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(using mass erase / erase-all-blocks command)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 20:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163874#M833</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2011-08-31T20:43:19Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163875#M834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for this specific clarification on Rev's.&amp;nbsp; I don't think the 1.4 enhancements will help my attempts to use this mechanism to support a bootloader, and the 'reliable' update desires thereof.&amp;nbsp; The flag words within each image still create difficulties.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would also like to remind anybody looking at these silicon changes that the change to the swap mechanism from the 'old' RTC_CCR register at offset 0x1C in RTC space in 1.0 silicon came with a change to that register definition!&amp;nbsp; It is now a RealTimeClock_InterruptEnableRegister at the same 0x1C offset, so operations at the 'old' CCR assumptions will mess with RTC interrupts you may be trying to use.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Earl Goodrich II&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2011 20:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163875#M834</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2011-08-31T20:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163876#M835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What code do you use to take the swap system from "uninitialized" to UPDATE-ERASED?&lt;/P&gt;&lt;P&gt;I tried the following register values but it did not work. Any suggestions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem:&amp;nbsp; An FTFL_FSTAT ACCERR violation occurs when the ”Initialize Swap System to UPDATE_ERASED State” FTFL command is issued.&lt;/P&gt;&lt;P&gt;FTFL is functional for programming and erasing FLASH as Flash copy routines can copy from Flash Bank 0 to Flash Bank 0 and from Flash Bank 0 to Flash bank 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;The “Report Swap System Status” SWAP system command reports the K60 is&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In the “Uninitialized State”&lt;/LI&gt;&lt;LI&gt;Current Flash bank is 0&lt;/LI&gt;&lt;LI&gt;Next swap bank is zero.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Note: An ACCERR is not issued when this command is executed&lt;/P&gt;&lt;P&gt;The FTFL registers are set as follows for the Initialize Swap System to UPDATE-ERASED state:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB0 = 0x46;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* The opcode for performing a FLASH Swap */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB1 = 0x03;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Use 0x3FFF0 as the “Swap Indicator” address */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB2 = 0xFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB3 = 0xF0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB4 = 0x01;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialize the Swap System&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/P&gt;&lt;P&gt;Then a ram function is called to clear CCIF by writing a ‘1’ to the bit. FTFL_STAT changes to 0xA0 immediately after clearing CCIF which indicates an ACCERR condition.&lt;/P&gt;&lt;P&gt;Addresses other than 0x03FFF0 were tried, 0x30000, 0x20000, and 0x10000, all with the same result.&lt;/P&gt;&lt;P&gt;Flash at 0x3FFF0- 0x3FFFF and 0x7FFF0 – 7FFFF are 0xFFs.&lt;/P&gt;&lt;P&gt;The Swap Indicator address is phrase aligned and in the lower FLASH bank but not in the Flash Configuration Field. The Swap system reports it is in UNITITIALIZED state. I believe all conditions have been properly met.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2012 03:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163876#M835</guid>
      <dc:creator>Zack</dc:creator>
      <dc:date>2012-01-20T03:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163877#M836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the mask code on your chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2012 04:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163877#M836</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-01-20T04:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163878#M837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mask code is 4N30D. I belive that is Rev 1.4 silicon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2012 05:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163878#M837</guid>
      <dc:creator>Zack</dc:creator>
      <dc:date>2012-01-20T05:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163879#M838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sounds like it.&amp;nbsp; I haven't tried since 1.2, so maybe it is different again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2012 06:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163879#M838</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-01-20T06:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163880#M839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For reference, this is the code I started to write to test/initialize the new swap mechanism, which 'bricked' my 1.2 part (which means it set up the swap mechanism, which I then couldn't use for my purposes, and in that rev was irreversable).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I BELIEVE this sequence will set address 0x3F0 (and the mirror address at 0x403F0 in the other bank) for the swap system flags.&amp;nbsp; I don't know if this is a particularly 'good' address to use, but note that whatever address you dedicate for this specifically protects the enclosing sector from erase activity except in the very specific sequence to run from one bank and erase the other in prep for this whole update-then-swap scenario.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if( (fnFlashNow(FCMD_SWAP_CONTROL, 0x3F0, 0x08FF) &amp;amp; FTFL_FSTAT_MGSTAT0_MASK) == 0 )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;//Command 8 == report swap status&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(FTFL_FCCOB5 == 0 )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnFlashNow(FCMD_SWAP_CONTROL, 0x3F0, 0x01FF); //'virgin', initialize swap system&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Command&amp;nbsp;1 == set swap indicator address&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if(FTFL_FCCOB5 == 1 ) //'Normal' ready state -- swap process NOT started&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; { //FTFL_FCCOB6 indicates which block is at address 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else //If we had a reset while the swap state machine was not 'Ready', we can't count on the new image&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else //Nonzero MGSTAT0 bit indicates some kind of fault during a swap-command execution&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;static int fnFlashNow(uint8_t ucCommand, uint32_t ptrWord, uint32_t ulWord)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; do{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }while (!(FTFL_FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)); // wait for previous commands to complete&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (FTFL_FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; { // check for errors in previous command&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FSTAT = (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK); // clear old errors&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; switch (FTFL_FCCOB0 = ucCommand) { // enter the command sequence&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case FCMD_ERASE_ALL_BLOCKS: // single command word required with the erase all blocks command&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case FCMD_SWAP_CONTROL:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB6 = 0xFF; //Clear these status bytes, in case of fault&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB7 = 0xFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case FCMD_PROGRAM_SECTION:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if( ucCommand == FCMD_PROGRAM_SECTION )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ulWord &amp;gt;&amp;gt;= 3; //Convert to dual-dword count&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB4 = (uint8_t)(ulWord &amp;gt;&amp;gt; 8);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB5 = (uint8_t)(ulWord);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;case FCMD_ERASE_FLASH_SECTOR:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB1 = (uint8_t)(ptrWord &amp;gt;&amp;gt; 16);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB2 = (uint8_t)(ptrWord &amp;gt;&amp;gt; 8);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FCCOB3 = (uint8_t)ptrWord;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Disable_Interrupt(); // protect this region from interrupts&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFL_FSTAT = FTFL_FSTAT_CCIF_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// launch the command - this clears the FTFL_STAT_CCIF flag (register is&amp;nbsp;FTFL_FSTAT)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (!(FTFL_FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)) {} // wait for the command to terminate&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return (FTFL_FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK | FTFL_FSTAT_MGSTAT0_MASK)); // if there was an error this will be non-zero&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2012 22:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163880#M839</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-01-20T22:57:42Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163881#M840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the code. It looks like my code does what your code does. The problem remains.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2012 22:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163881#M840</guid>
      <dc:creator>Zack</dc:creator>
      <dc:date>2012-01-23T22:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163882#M841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can see only two particular differences.&amp;nbsp; My code presets FCCOB5/6/7 to 0xFF prior to each command, per the note preceding Table 28-66.&amp;nbsp; Second, I let the IAR linker run my entire bootloader from RAM to avoid ANY bank access conflicts.&amp;nbsp; I have no idea how the 'initialize' command interacts with Flash banks, if at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I might get brave and try this process on a new 1.4 part, on the expectation the 'erase all' will reset it all for me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--ERGII&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2012 11:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163882#M841</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-01-24T11:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163883#M842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, I breakpoint my code just after the call to SWAP status, and the virgn state leads to the call to init, and afterwards the FCCOB reads:&lt;/P&gt;&lt;P&gt;460003f0 01030000&lt;/P&gt;&lt;P&gt;and the byte at 0x3F4 is cleared to zero.&lt;BR /&gt;If I reset and run to that breakpoint again, the status returned is now:&lt;/P&gt;&lt;P&gt;460003f0 08030000&lt;/P&gt;&lt;P&gt;which appears to mean, in both cases, that I am in state 'Update erased'.&lt;/P&gt;&lt;P&gt;Attempts now to upload full code thru JTAG find the affected sectors write protected, and the IAR upload is severely unhappy.&lt;BR /&gt;Fortunately for me, this 1.4 silicon does indeed respond to 'unlock kinetis' and returns to a programmable state, and Swap status is back to zero.&lt;/P&gt;&lt;P&gt;So, without developing the whole ping/pong process further, it looks like what I have works as advertised.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--ERGII&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2012 00:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163883#M842</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-01-25T00:18:42Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163884#M843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I've experinced the exact same problem described by Zack on a Rev 1.4 k10, MK10 DN512 ZVLQ 10, 144 pin. Program flash only, meaning it should support it, right?&lt;BR /&gt;&lt;BR /&gt;I use address 0x500 as swap indicator, alignment ok, not in Configuration fields and bank0.&lt;BR /&gt;After trying to init I get FTFL_STAT changes to 0xa0 an ACCERR condition as Zack mentioned. I did read resource and IFR in bank 0 say, 0x0500 FFFF. The status bits FCCOB5-7 get 0'ed.&lt;BR /&gt;&lt;BR /&gt;Did anyone get past those kind of problems&lt;BR /&gt;&lt;BR /&gt;//rtlaka&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2012 04:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163884#M843</guid>
      <dc:creator>rtlaka</dc:creator>
      <dc:date>2012-04-06T04:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163885#M844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You say 'address 0x500 in bank 0' for the indicator, but of course this new Kinetis mechanism also involves offset 0x500 in Bank 1 as the indicator for that bank, and that area must ALSO be erased prior to initializing the swap mechanism.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You didn't supply any full command sequences -- is your code following more-or-less exactly the codes, FCCB contents and status checks as my code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, since this swap initialization writes to BOTH flash banks, the commands MUST run from RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Egoodii&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2012 04:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163885#M844</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-04-06T04:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163886#M845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have the same FCCB sequence, more or less. I think the problem is erase related then.&lt;BR /&gt;&lt;BR /&gt;If I've never succesfully Init swap , do I need to run Erase-All-Blocks? The IFR seems to have been modified with the correct address but still UnInit 0xFFFF&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2012 15:32:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163886#M845</guid>
      <dc:creator>rtlaka</dc:creator>
      <dc:date>2012-04-06T15:32:38Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163887#M846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately, I can't really use this new swap mechanism, so I can't really be an 'expert' on the exact requirements.&amp;nbsp; The placement of these two 'status flag bytes', one each in each bank WITHIN processor address space makes a real complication to my environment where I need 90% of the flash for my application size.&amp;nbsp; This is TRULY meant to only work for the ping-pong one-actve/one-backup application images in flash, not with&amp;nbsp;the 'small bootloader' approach.&amp;nbsp; Now if they would've just put those flags in some other 'extra' flash space (like iFR!) I wouldn't have this memory map problem...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That being said, I can only know that the phrases each containing this flag byte, at the offset you specify in both banks,&amp;nbsp;must be&amp;nbsp;erased before you run the 'init' command to place the flash-update mechanism in this whole ping-pong-swap mode.&amp;nbsp; I went with 0x3f4 in my example simply because there is a 'hole' between the top of usable vectors and the config space that is otherwise difficult to use (and easy to see that the linker is 'ignoring').&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For my money, I would certainly start out with an empty chip, in fact I would go so far as to start with that 'mass erase' as with Jlink 'unlock kinetis' to insure the swap mechanism is un-initialized to start with, and as in my code will return such a status.&amp;nbsp; If you can't then 'init swap' I will have to assume it is a bank conflict due to processor-access to either bank during init.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, you haven't said but I assume you are running Rev 1.4 silicon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--ERGII&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2012 19:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163887#M846</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-04-06T19:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163888#M847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm running Rev 1.4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems it was erase related, to confirm I created a swap section size 2K that I erased just before Init. Then it worked.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My original code and idea was to keep a size 0x4 area free of code in the text section from the linker script to be used as swap indicator, I assumed it would work due to the fact I kept it 0xFF by FILL(0xFF). But seems it didn't&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//rtlaka&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2012 19:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163888#M847</guid>
      <dc:creator>rtlaka</dc:creator>
      <dc:date>2012-04-10T19:42:52Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163889#M848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have no particular proof, but I have a feeling the swap-flags need to reserve a whole phrase.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2012 01:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163889#M848</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-04-11T01:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: New Kinetis Flash SWAP mechanism</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163890#M849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What do you consider as the proper reset procedure to get the new swap running?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I implemented the warmreset I found on this forum, eg. writing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; read_value &amp;amp;= ~AIRCR_VECTKEY_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; read_value |= (AIRCR_VECTKEY(AIRCR_VECTKEY_WRITEKEY) | AIRCR_SYSRESETREQ);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//rtlaka&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2012 16:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/New-Kinetis-Flash-SWAP-mechanism/m-p/163890#M849</guid>
      <dc:creator>rtlaka</dc:creator>
      <dc:date>2012-04-11T16:01:18Z</dc:date>
    </item>
  </channel>
</rss>