<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KL25Z can't wake up from VLLSx mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-can-t-wake-up-from-VLLSx-mode/m-p/265643#M8557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I use FRDM Kl25Z, and processor expert with CW10.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I try to wake up from VLLSx mode via external pins P5, P6, P14, P15.&lt;/P&gt;&lt;P&gt;But it won't go to Cpu_OnLLSWakeUpINT() when I active the external pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I also try to wake up frome LLS mode via the external pin.&lt;/P&gt;&lt;P&gt;It could go to Cpu_OnLLSWakeUpINT() when I ative the external pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any body coud help me to resolve this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean Wu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jul 2013 02:01:37 GMT</pubDate>
    <dc:creator>seanwu</dc:creator>
    <dc:date>2013-07-11T02:01:37Z</dc:date>
    <item>
      <title>KL25Z can't wake up from VLLSx mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-can-t-wake-up-from-VLLSx-mode/m-p/265643#M8557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I use FRDM Kl25Z, and processor expert with CW10.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I try to wake up from VLLSx mode via external pins P5, P6, P14, P15.&lt;/P&gt;&lt;P&gt;But it won't go to Cpu_OnLLSWakeUpINT() when I active the external pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I also try to wake up frome LLS mode via the external pin.&lt;/P&gt;&lt;P&gt;It could go to Cpu_OnLLSWakeUpINT() when I ative the external pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any body coud help me to resolve this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean Wu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 02:01:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-can-t-wake-up-from-VLLSx-mode/m-p/265643#M8557</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2013-07-11T02:01:37Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z can't wake up from VLLSx mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-can-t-wake-up-from-VLLSx-mode/m-p/265644#M8558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When KL25 enter into LLS or VLLSx&amp;nbsp; low power mode, the GPIO module is static and pins latched.&lt;/P&gt;&lt;P&gt;It need to use LLWU module to wake up the chip from LLS or VLLSx&amp;nbsp; low power mode.&lt;/P&gt;&lt;P&gt;You can download and refer KL25_SC example code about low power mode:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/KL25_SC.exe"&gt;http://cache.freescale.com/files/32bit/software/KL25_SC.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 05:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-can-t-wake-up-from-VLLSx-mode/m-p/265644#M8558</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-07-11T05:36:43Z</dc:date>
    </item>
  </channel>
</rss>