<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using a thermistor with the FRDM board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263759#M8292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To add, I am using console printf's to send out what the ADC is reading, every 3 seconds or so.&amp;nbsp; I have played with that value quite a bit as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Apr 2013 01:40:33 GMT</pubDate>
    <dc:creator>steve_fae</dc:creator>
    <dc:date>2013-04-12T01:40:33Z</dc:date>
    <item>
      <title>Using a thermistor with the FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263758#M8291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Trying to accurately measure the temperature of a heat sink using the KL25 FRDM board with an attached daughter card.&amp;nbsp; The thermistor is a 10K series from Vishay and so I bias it to 3v and use a pull down resistor recommended by Vishay.&amp;nbsp; I need to measure within a few degrees of accuracy from 70deg C to 100deg C.&amp;nbsp; The problem is the ADC bounces all over the place.&amp;nbsp; I have tried averaging, throwing out an errant reading, etc.&amp;nbsp; but I still do not have a stable solution.&amp;nbsp; I capture 16 bits from the ADC then throw out the least 4 bits.&amp;nbsp; I even tried to look at just 8 bits of accuracy.&amp;nbsp; Is there something I am missing?&lt;/P&gt;&lt;P&gt;Also I only need to capture 32 steps along that range.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119242i7D809E5A5D42C042/image-size/large?v=v2&amp;amp;px=999" title="3845_3845.png" alt="3845_3845.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 01:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263758#M8291</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-04-12T01:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: Using a thermistor with the FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263759#M8292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To add, I am using console printf's to send out what the ADC is reading, every 3 seconds or so.&amp;nbsp; I have played with that value quite a bit as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 01:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263759#M8292</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-04-12T01:40:33Z</dc:date>
    </item>
    <item>
      <title>Re: Using a thermistor with the FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263760#M8293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve,&lt;/P&gt;&lt;P&gt;Which ADC channel/pin are you using and how are you configuring the ADC module and sample rate?&lt;/P&gt;&lt;P&gt;Have you tried connecting to another source? Also testing to VCC and GND.&lt;/P&gt;&lt;P&gt;Are you using other ADC channel/pin combinations too?&amp;nbsp; If yes try only sampling your temp sensor and not the other stuff.&lt;/P&gt;&lt;P&gt;Any wiring issues?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 19:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263760#M8293</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-04-12T19:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: Using a thermistor with the FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263761#M8294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is the configuration.&amp;nbsp; The core is running at 20 Mhz btw. &lt;/P&gt;&lt;P&gt;I think that the folks at Vishay let me astray.&amp;nbsp; I had asked if I needed any additional caps/resistors on the thermistor and they said no.&amp;nbsp; I found this diagram at the Arduino Playground showing some nice bulk caps on VCC as well as at the center point of the thermistor connection.&amp;nbsp; Hooking up the caps really calmed things down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39202i1237D33F06B5D2D0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39201i8B59A1FC440F3EA2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Apr 2013 03:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263761#M8294</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-04-13T03:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Using a thermistor with the FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263762#M8295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve,&lt;/P&gt;&lt;P&gt;Great news.&amp;nbsp; Good digging into the issue and thanks for letting us know the solution.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Apr 2013 18:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-a-thermistor-with-the-FRDM-board/m-p/263762#M8295</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-04-13T18:36:49Z</dc:date>
    </item>
  </channel>
</rss>