<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis USB detailed hardware manual</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263618#M8290</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to implement a composite device that has 5 ccid smartcard readers and 1 hid interface. I believe I need to write my own class drivers, although I could use the hid drivers from the example projects. However, I would like to know the internal working of the USB peripheral and the things done in USB_LLD code from a USB device perspective. The reference manual just touches up on these details but it is not giving a full description of the how the USB peripheral works. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sure there would be some resource available but it may be internal to FSL. Anyway, I thought it is worth asking.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Ismail&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Dec 2013 09:09:30 GMT</pubDate>
    <dc:creator>izmile</dc:creator>
    <dc:date>2013-12-17T09:09:30Z</dc:date>
    <item>
      <title>Kinetis USB detailed hardware manual</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263616#M8288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello folks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a new kinetis user. I was wondering if there is a detailed hardware description of the USB peripheral used in Kinetis processors. I got the USB OTG/Host/Device stack user manual and the reference manual of the processor (K60) that I am using. However, I believe it does not cover all the details. There are lot more things done in USB_LDD code, than what is given in the reference manual. Any pointers would be of great help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Ismail&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2013 09:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263616#M8288</guid>
      <dc:creator>izmile</dc:creator>
      <dc:date>2013-12-16T09:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis USB detailed hardware manual</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263617#M8289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ismail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What class you want to use? There are some example projects in Freescale USB stack 4.1.1. It can help you to get a start. After you install, you can find in folder path C:\Freescale\Freescale USB Stack v4.1.1\ProcessorExpert\Examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 06:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263617#M8289</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-12-17T06:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis USB detailed hardware manual</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263618#M8290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to implement a composite device that has 5 ccid smartcard readers and 1 hid interface. I believe I need to write my own class drivers, although I could use the hid drivers from the example projects. However, I would like to know the internal working of the USB peripheral and the things done in USB_LLD code from a USB device perspective. The reference manual just touches up on these details but it is not giving a full description of the how the USB peripheral works. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sure there would be some resource available but it may be internal to FSL. Anyway, I thought it is worth asking.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Ismail&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 09:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-detailed-hardware-manual/m-p/263618#M8290</guid>
      <dc:creator>izmile</dc:creator>
      <dc:date>2013-12-17T09:09:30Z</dc:date>
    </item>
  </channel>
</rss>