<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: LLWU on KL14 problems</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLWU-on-KL14-problems/m-p/263542#M8278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.&lt;/P&gt;&lt;P&gt;So, It is not clear the documentation error reported in this discussion:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-objectid="319868" data-objecttype="2" href="https://community.nxp.com/message/319868#319868" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #6a737b;"&gt;https://community.freescale.com/message/319868#319868&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Nov 2013 08:06:58 GMT</pubDate>
    <dc:creator>ulivinico</dc:creator>
    <dc:date>2013-11-08T08:06:58Z</dc:date>
    <item>
      <title>LLWU on KL14 problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLWU-on-KL14-problems/m-p/263541#M8277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've developed an application with KL25 by using the evaluation board FRDM that makes use of wakeup from low power mode by using LLWU_P5/PTB0. Everything works well. &lt;/P&gt;&lt;P&gt;Then I've ported the program to KL14 and everything works except the wakeup on that pin. &lt;/P&gt;&lt;P&gt;I read here: &lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/319868#319868"&gt;https://community.freescale.com/message/319868#319868&lt;/A&gt;&lt;/P&gt;&lt;P&gt;that there is errors in documentation and LLWU interrupts on port B doesn't work. Is this true? &lt;/P&gt;&lt;P&gt;Is it not possible use the PTB0 as wakeup pin? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2013 08:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLWU-on-KL14-problems/m-p/263541#M8277</guid>
      <dc:creator>ulivinico</dc:creator>
      <dc:date>2013-11-07T08:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: LLWU on KL14 problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLWU-on-KL14-problems/m-p/263542#M8278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: The malfunction was due to an hardware problem of my board. Wakeup by LLWU pin is working on Port B as well in KL14.&lt;/P&gt;&lt;P&gt;So, It is not clear the documentation error reported in this discussion:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-objectid="319868" data-objecttype="2" href="https://community.nxp.com/message/319868#319868" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #6a737b;"&gt;https://community.freescale.com/message/319868#319868&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2013 08:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLWU-on-KL14-problems/m-p/263542#M8278</guid>
      <dc:creator>ulivinico</dc:creator>
      <dc:date>2013-11-08T08:06:58Z</dc:date>
    </item>
  </channel>
</rss>