<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Extract SerialNumber File from Cyclone in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extract-SerialNumber-File-from-Cyclone/m-p/263189#M8236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Cyclone Max for burn Kinetis devices, and autogenerate serial numbers with it. I use the file .se created with "Serialize" software tool for generate the first number and the structure. But I have a question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to extract this "serial file" from Cyclone Max when I need to put another SAP file in? When I erase the SAP file, I need to regenerate the file with the last serial number using serialize, and put it in the compilation again. It is possible to save it FROM the Cyclone for not regenerate the .ser file with the "Serialize" tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Miguel Ángel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Oct 2013 16:19:59 GMT</pubDate>
    <dc:creator>night</dc:creator>
    <dc:date>2013-10-03T16:19:59Z</dc:date>
    <item>
      <title>Extract SerialNumber File from Cyclone</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extract-SerialNumber-File-from-Cyclone/m-p/263189#M8236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Cyclone Max for burn Kinetis devices, and autogenerate serial numbers with it. I use the file .se created with "Serialize" software tool for generate the first number and the structure. But I have a question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to extract this "serial file" from Cyclone Max when I need to put another SAP file in? When I erase the SAP file, I need to regenerate the file with the last serial number using serialize, and put it in the compilation again. It is possible to save it FROM the Cyclone for not regenerate the .ser file with the "Serialize" tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Miguel Ángel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2013 16:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Extract-SerialNumber-File-from-Cyclone/m-p/263189#M8236</guid>
      <dc:creator>night</dc:creator>
      <dc:date>2013-10-03T16:19:59Z</dc:date>
    </item>
  </channel>
</rss>