<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Wrong input voltage levels Kinetis K10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262583#M8219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply! Now when you say it it sounds logical.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bosse &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jan 2014 07:34:42 GMT</pubDate>
    <dc:creator>bostångberg</dc:creator>
    <dc:date>2014-01-31T07:34:42Z</dc:date>
    <item>
      <title>Wrong input voltage levels Kinetis K10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262581#M8217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, all!&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I am using the MK10DX128VLL7 kinetis processor. And have some problems with the GPIO input voltage levels.&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The supply voltage is 3,3V and if i look in K10P100M72SF1 document table 1 the levels are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Input high voltage Min 0.7*3.3V = 2.31V.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Input low voltage Max 0.35*3.3V = 1.155V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i measure on my prototype board the levels spreads and are not as the datasheet says.&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PTB0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Input high voltage 1,78V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Input low voltage 1,7V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;PTD2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Input high voltage 1,74V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Input low voltage 1,3V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The input high voltage level seems to be around 1,7-1,8V for all pins but the low voltage level spreds all from 1.15V to 1.7V. There is no spikes and the supply voltage looks good.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Has anyone any idea why the levels are not as datasheet says?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 15:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262581#M8217</guid>
      <dc:creator>bostångberg</dc:creator>
      <dc:date>2014-01-28T15:38:39Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong input voltage levels Kinetis K10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262582#M8218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as you mensioned the datasheet says about the input ranges that Input low voltage Max is 1.155V and Input high voltage Min is 2.31V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These informations mean that in the range between 1.155 V to 2.31 V is not guaranteed the correct logical level of the input signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guaranteed:&lt;/P&gt;&lt;P&gt;0 V -&amp;gt; 1.155 V&amp;nbsp; = logical 0&lt;/P&gt;&lt;P&gt;2.31 V -&amp;gt; 3.3 V = logical 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2014 07:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262582#M8218</guid>
      <dc:creator>pavel_krenek</dc:creator>
      <dc:date>2014-01-30T07:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong input voltage levels Kinetis K10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262583#M8219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply! Now when you say it it sounds logical.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bosse &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2014 07:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wrong-input-voltage-levels-Kinetis-K10/m-p/262583#M8219</guid>
      <dc:creator>bostångberg</dc:creator>
      <dc:date>2014-01-31T07:34:42Z</dc:date>
    </item>
  </channel>
</rss>