<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FlexCan Kinetis K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-FlexCan-Kinetis-K70/m-p/261843#M8132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the CAN Phy is a half duplex, it can't send ACK signal during CAN message transfer.&lt;BR /&gt;So, the K70 FlexCAN module doesn't receive the ACK signal will send CAN message again until this CAN node off line.&lt;BR /&gt;It need another CAN node on bus to provide the ACK signal.&lt;BR /&gt;If only one CAN node, customer need to use FlexCAN loop-back mode.&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jan 2014 08:21:32 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2014-01-13T08:21:32Z</dc:date>
    <item>
      <title>Re: FlexCan Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-FlexCan-Kinetis-K70/m-p/261843#M8132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the CAN Phy is a half duplex, it can't send ACK signal during CAN message transfer.&lt;BR /&gt;So, the K70 FlexCAN module doesn't receive the ACK signal will send CAN message again until this CAN node off line.&lt;BR /&gt;It need another CAN node on bus to provide the ACK signal.&lt;BR /&gt;If only one CAN node, customer need to use FlexCAN loop-back mode.&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 08:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Re-FlexCan-Kinetis-K70/m-p/261843#M8132</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-01-13T08:21:32Z</dc:date>
    </item>
  </channel>
</rss>