<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCGOUTCLK Up to 120MHz? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCGOUTCLK-Up-to-120MHz/m-p/261490#M8116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I assume you speak of a 120MHz-rated K20 part.&amp;nbsp; For the functions performed by MCGOUTCLK, said part-rating is certainly 'the legal limit'.&amp;nbsp; The fact that an example in the RM (25.5.3.1) is 'not usable' by a particular chip is just a weakness of the manual-editors, much like the 100MHz 'Fsys' factor used throughout the SPI chapter, despite the fact that the 'fastest available' Kinetis bus clock is 75MHz.&amp;nbsp; 'Actually usable' examples would certainly always be preferable...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case, there are some K60/61/70 parts rated at 150Mhz to net your 144MHz 'fully legal'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jan 2014 18:53:35 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2014-01-29T18:53:35Z</dc:date>
    <item>
      <title>MCGOUTCLK Up to 120MHz?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCGOUTCLK-Up-to-120MHz/m-p/261489#M8115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the following questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in K20 Sub-Family Reference Manual, Rev. 2, Dec 2011&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.[5.4.1 Device clock summary Table 5-1. Clock Summary]&lt;/P&gt;&lt;P&gt;"MCGOUTCLK" is "Up to 120 MHz".&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;But, I want to output 144MHz from "MCGOUTCLK" using PLL0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;It is setable, is it out of a guarantee?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;2.[&lt;/SPAN&gt;25.5.3.1 "MCGOUTCLK Frequency = 128 MHz"]&lt;/P&gt;&lt;P&gt;Is it out of a guarantee?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 06:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCGOUTCLK-Up-to-120MHz/m-p/261489#M8115</guid>
      <dc:creator>okubohitoshi</dc:creator>
      <dc:date>2014-01-28T06:24:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCGOUTCLK Up to 120MHz?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCGOUTCLK-Up-to-120MHz/m-p/261490#M8116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I assume you speak of a 120MHz-rated K20 part.&amp;nbsp; For the functions performed by MCGOUTCLK, said part-rating is certainly 'the legal limit'.&amp;nbsp; The fact that an example in the RM (25.5.3.1) is 'not usable' by a particular chip is just a weakness of the manual-editors, much like the 100MHz 'Fsys' factor used throughout the SPI chapter, despite the fact that the 'fastest available' Kinetis bus clock is 75MHz.&amp;nbsp; 'Actually usable' examples would certainly always be preferable...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case, there are some K60/61/70 parts rated at 150Mhz to net your 144MHz 'fully legal'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2014 18:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCGOUTCLK-Up-to-120MHz/m-p/261490#M8116</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-01-29T18:53:35Z</dc:date>
    </item>
  </channel>
</rss>