<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Changing hardware connection in CW Kinetis Project</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260493#M7969</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can create a new connection like in your screen attached, completing the target device and the hardware debugger interface or just change the hw in the segger existing connection. Go to debug configurations &amp;gt; Select the configuration for Segger &amp;gt; press Edit button and in the Connection Type, select P&amp;amp;E instead of Jlink.&lt;/P&gt;&lt;P&gt;That's all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2013 18:23:52 GMT</pubDate>
    <dc:creator>LuisCasado</dc:creator>
    <dc:date>2013-02-15T18:23:52Z</dc:date>
    <item>
      <title>Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260492#M7968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project that was built with a Segger Jlink for hardware connection.&amp;nbsp; I only have access to OSBDM or a PEMicro universal multilink.&amp;nbsp; Is there a script to follow in order to modify the project settings to change the build to use what I have access to?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am stuck at this stage.&amp;nbsp; I don't know how to import something from lets say a project that is already configured correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="3266_3266.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119096i853AC7394BBFE39E/image-size/large?v=v2&amp;amp;px=999" role="button" title="3266_3266.png" alt="3266_3266.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 18:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260492#M7968</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-02-15T18:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260493#M7969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can create a new connection like in your screen attached, completing the target device and the hardware debugger interface or just change the hw in the segger existing connection. Go to debug configurations &amp;gt; Select the configuration for Segger &amp;gt; press Edit button and in the Connection Type, select P&amp;amp;E instead of Jlink.&lt;/P&gt;&lt;P&gt;That's all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 18:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260493#M7969</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2013-02-15T18:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260494#M7970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Luis, I still can't connect to the target but I am sure that's because I have an LCD connected to the tower and need an external power supply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 19:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260494#M7970</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-02-15T19:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260495#M7971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;so I changed the settings from jlink to PE multilink but it won't connect&lt;/P&gt;&lt;P&gt;first captures shows setting second shows connection error&lt;/P&gt;&lt;P&gt;what i have in hand is a universal multilink but it seems to have found an FX??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="3270_3270.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119094iF4C8EA54092BC574/image-size/large?v=v2&amp;amp;px=999" role="button" title="3270_3270.png" alt="3270_3270.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="3271_3271.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119095iDE16B23A026A22AF/image-size/large?v=v2&amp;amp;px=999" role="button" title="3271_3271.png" alt="3271_3271.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 22:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260495#M7971</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-02-15T22:58:18Z</dc:date>
    </item>
    <item>
      <title>Re: Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260496#M7972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connection configuration looks ok. Do you have the two Multilik led's on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can do two things:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Create a new project with CW wizard and try to connect.&lt;/P&gt;&lt;P&gt;2) Enable log in debug connection to see what error is reported&lt;/P&gt;&lt;P&gt;How are you powering the TWR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2013 18:19:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260496#M7972</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2013-02-16T18:19:08Z</dc:date>
    </item>
    <item>
      <title>Re: Changing hardware connection in CW Kinetis Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260497#M7973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, using straight usb connection with OSJTAG I got a connection.&amp;nbsp; Now need to get panel to light up.&amp;nbsp; Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Feb 2013 04:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Changing-hardware-connection-in-CW-Kinetis-Project/m-p/260497#M7973</guid>
      <dc:creator>steve_fae</dc:creator>
      <dc:date>2013-02-17T04:58:38Z</dc:date>
    </item>
  </channel>
</rss>