<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM-KL05Z not working,no SWD activity launching debug</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260001#M7933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;please can i have your help?&lt;/P&gt;&lt;P&gt;i unseccessfully tried to use the freedom board FRDM-KL05Z as a tool for programming an external device.&lt;/P&gt;&lt;P&gt;Now i need to use it with it's resident processor, i restored the board as it was,(2 cutted tracks restored) but it does not works at all.&lt;/P&gt;&lt;P&gt;In mass storage mode, i dragged in the "JLink_OpenSDA.sda" file,and ,after plugged once more in the USB , the board appears to the PC&amp;nbsp; Control panel..-&amp;gt;Device Manager-&amp;gt;Controller USB, as " J-Link driver".So no doubt that XP is aware of the board.&lt;/P&gt;&lt;P&gt;Then I load a complete example project: "kl05_frdm_demo".Once built i launch debug,;I can choose 2 different options,I choose J-Link/J-Trace for ARM,Ok,launched,,but the progress bar stucks at 61%,and i need to push the red button to stop it.&lt;/P&gt;&lt;P&gt;It is the same behaviour that i have when i launch it &lt;STRONG&gt;with no USB cable&lt;/STRONG&gt;.It looks very strange that i'm not warned that USB is unconnected.&lt;/P&gt;&lt;P&gt;If i check on oscilloscope, SWD signals are inactive,as one should expect &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Diego&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jan 2014 16:34:01 GMT</pubDate>
    <dc:creator>diegocolombo</dc:creator>
    <dc:date>2014-01-27T16:34:01Z</dc:date>
    <item>
      <title>FRDM-KL05Z not working,no SWD activity launching debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260001#M7933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;please can i have your help?&lt;/P&gt;&lt;P&gt;i unseccessfully tried to use the freedom board FRDM-KL05Z as a tool for programming an external device.&lt;/P&gt;&lt;P&gt;Now i need to use it with it's resident processor, i restored the board as it was,(2 cutted tracks restored) but it does not works at all.&lt;/P&gt;&lt;P&gt;In mass storage mode, i dragged in the "JLink_OpenSDA.sda" file,and ,after plugged once more in the USB , the board appears to the PC&amp;nbsp; Control panel..-&amp;gt;Device Manager-&amp;gt;Controller USB, as " J-Link driver".So no doubt that XP is aware of the board.&lt;/P&gt;&lt;P&gt;Then I load a complete example project: "kl05_frdm_demo".Once built i launch debug,;I can choose 2 different options,I choose J-Link/J-Trace for ARM,Ok,launched,,but the progress bar stucks at 61%,and i need to push the red button to stop it.&lt;/P&gt;&lt;P&gt;It is the same behaviour that i have when i launch it &lt;STRONG&gt;with no USB cable&lt;/STRONG&gt;.It looks very strange that i'm not warned that USB is unconnected.&lt;/P&gt;&lt;P&gt;If i check on oscilloscope, SWD signals are inactive,as one should expect &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Diego&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2014 16:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260001#M7933</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2014-01-27T16:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL05Z not working,no SWD activity launching debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260002#M7934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A colleague made a tutorial on how to program different devices with the OpenSDA included in the FRDM-KL25Z. He tried with Cortex-M0+ (KL25 and KL05) and Cortex-M4 (K20 at 50MHz) and it worked. Please note that it works only for &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;programming&lt;/STRONG&gt;&lt;/SPAN&gt; purpose not for debugging purpose &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 00:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260002#M7934</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-01-28T00:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL05Z not working,no SWD activity launching debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260003#M7935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Please note that it works only for &lt;/SPAN&gt;&lt;SPAN class="&amp;amp;quothighlight&amp;quot;" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;STRONG style="font-style: inherit; font-family: inherit;"&gt;programming&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; purpose not for debugging purpose&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;Thank you for remark it,Soledad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately i discovered that the problem is at PC level,I tried with another PC,the FRDM board works fine.&lt;/P&gt;&lt;P&gt;30 days ago i got a virus,i cleaned it and i used CCLeaner to wipe out the PC,touching the configuration register.&lt;/P&gt;&lt;P&gt;By that day another IDE had the same problem,and now it happens that the debugger engine reaches the 61% and than it hangs,and it does'nt care at all about the presence of USB connection or less.&lt;/P&gt;&lt;P&gt;I reinstalled codewarrior,i reinstalled J-Link drivers,no way.&lt;/P&gt;&lt;P&gt;Please can i have some hints?&lt;/P&gt;&lt;P&gt;Now i try with system configuratione&amp;nbsp; restore&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 12:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL05Z-not-working-no-SWD-activity-launching-debug/m-p/260003#M7935</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2014-01-28T12:03:42Z</dc:date>
    </item>
  </channel>
</rss>