<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 UART2 on PTE22 &amp; PTE23</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259551#M7897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the freedom board with the Mbed compiler and am having trouble accessing UART2 on PTE22 &amp;amp; PTE23. I'm wondering if this is a problem with the compiler or something to do with the board? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not a show-stopper if I can't use the port but it would make the design a bit simpler. Any advice appreciated. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank, Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2013 02:26:24 GMT</pubDate>
    <dc:creator>ralphs</dc:creator>
    <dc:date>2013-05-28T02:26:24Z</dc:date>
    <item>
      <title>UART2 on PTE22 &amp; PTE23</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259551#M7897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the freedom board with the Mbed compiler and am having trouble accessing UART2 on PTE22 &amp;amp; PTE23. I'm wondering if this is a problem with the compiler or something to do with the board? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not a show-stopper if I can't use the port but it would make the design a bit simpler. Any advice appreciated. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank, Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 02:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259551#M7897</guid>
      <dc:creator>ralphs</dc:creator>
      <dc:date>2013-05-28T02:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: UART2 on PTE22 &amp; PTE23</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259552#M7898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried with CodeWarrior MCU V10.x software or IAR ARM Workbench?&lt;/P&gt;&lt;P&gt;You could use above IDE softwares to control FRDM-KL25Z UART2 pins.&lt;/P&gt;&lt;P&gt;Before operation PTE22 and PTE23 pins, it need to enable PORTE clock gate at SIM_SCGC5 register at first.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 05:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259552#M7898</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-05-28T05:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: UART2 on PTE22 &amp; PTE23</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259553#M7899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui_ma,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your comments. I haven't tried any other compilers, but I will.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers, Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 00:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART2-on-PTE22-PTE23/m-p/259553#M7899</guid>
      <dc:creator>ralphs</dc:creator>
      <dc:date>2013-05-29T00:23:38Z</dc:date>
    </item>
  </channel>
</rss>