<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックtwr-k60n512 ethernet phy</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twr-k60n512-ethernet-phy/m-p/258695#M7833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on the schematic diagram of &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;k60n512&lt;/SPAN&gt; demo-board the jtag connector debug traces' signals are connected to the microcontroller dedicated pins. This thing is possible because the uC is interfaced in RMMI mode with the ethernet PHY.&lt;/P&gt;&lt;P&gt;I want to use the MII interface signals instead, but MII0_RXD2 and MII0_RXD3 share the TRACE_D0 &amp;amp; TRACE_D1 pins.&lt;/P&gt;&lt;P&gt;How can i resolve this issue?&lt;/P&gt;&lt;P&gt;Can you help me with any suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 May 2013 13:46:22 GMT</pubDate>
    <dc:creator>franticcarlitos</dc:creator>
    <dc:date>2013-05-27T13:46:22Z</dc:date>
    <item>
      <title>twr-k60n512 ethernet phy</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twr-k60n512-ethernet-phy/m-p/258695#M7833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on the schematic diagram of &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;k60n512&lt;/SPAN&gt; demo-board the jtag connector debug traces' signals are connected to the microcontroller dedicated pins. This thing is possible because the uC is interfaced in RMMI mode with the ethernet PHY.&lt;/P&gt;&lt;P&gt;I want to use the MII interface signals instead, but MII0_RXD2 and MII0_RXD3 share the TRACE_D0 &amp;amp; TRACE_D1 pins.&lt;/P&gt;&lt;P&gt;How can i resolve this issue?&lt;/P&gt;&lt;P&gt;Can you help me with any suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 13:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/twr-k60n512-ethernet-phy/m-p/258695#M7833</guid>
      <dc:creator>franticcarlitos</dc:creator>
      <dc:date>2013-05-27T13:46:22Z</dc:date>
    </item>
    <item>
      <title>Re: twr-k60n512 ethernet phy</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/twr-k60n512-ethernet-phy/m-p/258696#M7834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi, Carlitos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you have two solution for your applicaiton. One is you can only use SWD lines: SWDIO, SWDCLK, /RESET, VDD, GND. You can also only use JTAG signals: TDI/TDO, TCK, TMS PLUS /RESET, VDD, GND. So you need not have to use trace data signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 01:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/twr-k60n512-ethernet-phy/m-p/258696#M7834</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-05-28T01:39:33Z</dc:date>
    </item>
  </channel>
</rss>