<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックBricked boards  Second phase</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258423#M7788</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After having problems with my first two FRDM boards I sent Freescale a fault report and they very kindly sent two replacements , these arrived this afternoon , keen to check them out I connected them to the USB lead on my main computer , running XP, both boards came up as "FRDM-KL25Z." as per the Quick Start Guide , all well and good , and the demo program showed that the accelerometers were functioning as expected , put them away and had dinner, I decided to try loading one of the precompiled srec&amp;nbsp; examples&amp;nbsp; , That's when the problems started , on plugging the USB lead ( without attempting to go into bootloader) After a short delay&amp;nbsp; I was presented&amp;nbsp; with the error message&amp;nbsp; " Delayed write failed " after which the board came up as "Invalid" rather than "FRDM-KL24Z"&amp;nbsp; or "Bootloader"&amp;nbsp;&amp;nbsp; Disconnecting and reconnecting it enumerated as "Bootloader" with no sign of the demo program and the green bootloader light flashing as per the original two that failed&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a check I did a "LSUSB" on one of my Linux boxes and note that the still working FRDM ID enumerates as "1357:0707 P&amp;amp;E Microcomputer systems" , the dead ones show as "2504:0200" , So it appears that something is wiping out the original&amp;nbsp; OpenSDA programming ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is starting to really bug me , it appears that something in my main computer XP system is killing FRDM boards ( 3 of 4 so far , and the fourth I'm very reticent to plug in to my main computer again, though it seems to behave on my XP laptop) ,&amp;nbsp; I have several Micro programming systems installed in the main computer&amp;nbsp; ( Arduino, Energia, Coocox,Espruino, Code composer etc ,)&amp;nbsp; but none of these are running while I'm playing with the Freedom boards&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any brilliant ideas before I tear what little remaining hair I have out ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Art&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Feb 2013 11:48:15 GMT</pubDate>
    <dc:creator>chop</dc:creator>
    <dc:date>2013-02-14T11:48:15Z</dc:date>
    <item>
      <title>Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258423#M7788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After having problems with my first two FRDM boards I sent Freescale a fault report and they very kindly sent two replacements , these arrived this afternoon , keen to check them out I connected them to the USB lead on my main computer , running XP, both boards came up as "FRDM-KL25Z." as per the Quick Start Guide , all well and good , and the demo program showed that the accelerometers were functioning as expected , put them away and had dinner, I decided to try loading one of the precompiled srec&amp;nbsp; examples&amp;nbsp; , That's when the problems started , on plugging the USB lead ( without attempting to go into bootloader) After a short delay&amp;nbsp; I was presented&amp;nbsp; with the error message&amp;nbsp; " Delayed write failed " after which the board came up as "Invalid" rather than "FRDM-KL24Z"&amp;nbsp; or "Bootloader"&amp;nbsp;&amp;nbsp; Disconnecting and reconnecting it enumerated as "Bootloader" with no sign of the demo program and the green bootloader light flashing as per the original two that failed&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a check I did a "LSUSB" on one of my Linux boxes and note that the still working FRDM ID enumerates as "1357:0707 P&amp;amp;E Microcomputer systems" , the dead ones show as "2504:0200" , So it appears that something is wiping out the original&amp;nbsp; OpenSDA programming ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is starting to really bug me , it appears that something in my main computer XP system is killing FRDM boards ( 3 of 4 so far , and the fourth I'm very reticent to plug in to my main computer again, though it seems to behave on my XP laptop) ,&amp;nbsp; I have several Micro programming systems installed in the main computer&amp;nbsp; ( Arduino, Energia, Coocox,Espruino, Code composer etc ,)&amp;nbsp; but none of these are running while I'm playing with the Freedom boards&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any brilliant ideas before I tear what little remaining hair I have out ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Art&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 11:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258423#M7788</guid>
      <dc:creator>chop</dc:creator>
      <dc:date>2013-02-14T11:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258424#M7789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probably as you said something is going wrong with your XP computer. I think you need to try with a different computer because it is not a normal behavior for more than 2 or 3 FRDM boards. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 16:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258424#M7789</guid>
      <dc:creator>adriansc</dc:creator>
      <dc:date>2013-02-14T16:05:52Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258425#M7790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm aware that some shell extensions (File Commander, etc) might cause issues. But to my knowledge the programming of the board failed, and should not brick the board. Not sure if you are using such an utility. Using the DOS shell/cmd 'copy' command to copy the file was working in these cases. Can you confirm that you did use 'copy' and not some kind of utility?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 16:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258425#M7790</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-02-14T16:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258426#M7791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Art,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have had a report that extensions to the Windows Explorer file manager can cause problems when trying to load images to the Freedom board. This could be possible since with a FAT file system, the PC could write the file in many different ways and it would valid for a real mass storage device but mis-understood by the Freedom board (for instance writing a file backwards or in random order). We are currently looking into this, and it may be what is affecting you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The good news is that the Bootloader is in protected memory, so you should be able to recover any of the boards. You have to put the Freedom board into Bootloader mode and then copy the appropriate MSD (mass storage application) to your Freedom board. The important part is, for now, not to use Windows Explorer to do this. Either use a different PC, or open a Command Prompt and use the "copy" command to copy the application to the board. All of the applications can be downloaded from &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.pemicro.com/opensda"&gt;http://www.pemicro.com/opensda&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will ask you off-line to send me the example project you tried programming into the unit so we can test that as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 16:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258426#M7791</guid>
      <dc:creator>kevin1</dc:creator>
      <dc:date>2013-02-14T16:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258427#M7792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 01:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258427#M7792</guid>
      <dc:creator>chop</dc:creator>
      <dc:date>2013-02-15T01:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258428#M7793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 01:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258428#M7793</guid>
      <dc:creator>chop</dc:creator>
      <dc:date>2013-02-15T01:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258429#M7794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had a board I thought was "bricked", plugging it in showed me the FRDM-KL25Z drive, but copying any application to it did nothing,&amp;nbsp; looking at laststat showed "programming" forever.&amp;nbsp; Then I found this:&lt;/P&gt;&lt;P&gt;Pemicro_OpenSDA_Debug_MSD_Update_Apps_2013_01_07 which contained a bootloader update and instructions.&lt;/P&gt;&lt;P&gt;Problem solved, board works fine again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 15:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258429#M7794</guid>
      <dc:creator>Tommy44</dc:creator>
      <dc:date>2013-02-15T15:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258430#M7795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please share where you found it?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 15:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258430#M7795</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2013-02-15T15:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258431#M7796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/support/downloads_find.cfm" target="test_blank"&gt;http://www.pemicro.com/support/downloads_find.cfm&lt;/A&gt; then look in the left &lt;/P&gt;&lt;P&gt;hand column for Open  SDA firmware applications"  Download it, unzip it &lt;/P&gt;&lt;P&gt;and read the bootloader update instructions.  I hope it works for you.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 18:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258431#M7796</guid>
      <dc:creator>Tommy44</dc:creator>
      <dc:date>2013-02-15T18:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258432#M7797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/opensda"&gt;www.pemicro.com/opensda&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119091i5FDBA455A367A84E/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 19:34:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258432#M7797</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2013-02-15T19:34:16Z</dc:date>
    </item>
    <item>
      <title>Re: Bricked boards  Second phase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258433#M7798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This solution also works for the FRDM-KL46Z board. I just tried it myself. Thanks for replying to the OP with the solution!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2013 12:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Bricked-boards-Second-phase/m-p/258433#M7798</guid>
      <dc:creator>carlosmendoza</dc:creator>
      <dc:date>2013-09-30T12:01:32Z</dc:date>
    </item>
  </channel>
</rss>