<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックTWR-K40X256 Reset</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K40X256-Reset/m-p/257195#M7631</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey, this is a very newbie question:&amp;nbsp; I ended up using some of the example programs to get familiar with the TWR-K40X256.&amp;nbsp; One of the tutorials i followed had the example program (flashing LED) sent to the flash memory instead of RAM.&amp;nbsp; Well, at some point something was corrupted and the program overwrote the demo program on board which has affected many things including coms.&amp;nbsp; Since it`s at the non volatile state we can`t remove it.&amp;nbsp; Is there a factory reset, such as moving a jumper on the board or a program that can reflash back to the factory demo which came onboard.&amp;nbsp; We think we have learned our lesson if we can just get back to a known working configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Apr 2013 18:17:53 GMT</pubDate>
    <dc:creator>billsorel</dc:creator>
    <dc:date>2013-04-08T18:17:53Z</dc:date>
    <item>
      <title>TWR-K40X256 Reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K40X256-Reset/m-p/257195#M7631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey, this is a very newbie question:&amp;nbsp; I ended up using some of the example programs to get familiar with the TWR-K40X256.&amp;nbsp; One of the tutorials i followed had the example program (flashing LED) sent to the flash memory instead of RAM.&amp;nbsp; Well, at some point something was corrupted and the program overwrote the demo program on board which has affected many things including coms.&amp;nbsp; Since it`s at the non volatile state we can`t remove it.&amp;nbsp; Is there a factory reset, such as moving a jumper on the board or a program that can reflash back to the factory demo which came onboard.&amp;nbsp; We think we have learned our lesson if we can just get back to a known working configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 18:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K40X256-Reset/m-p/257195#M7631</guid>
      <dc:creator>billsorel</dc:creator>
      <dc:date>2013-04-08T18:17:53Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K40X256 Reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K40X256-Reset/m-p/257196#M7632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You have to download the demo code to the board again.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/support_info/TWRK40X256QSDLAB.zip"&gt;http://cache.freescale.com/files/32bit/doc/support_info/TWRK40X256QSDLAB.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;see also: &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K40X256&amp;amp;tid=vanTWR-K40X256"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K40X256&amp;amp;tid=vanTWR-K40X256&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 08:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K40X256-Reset/m-p/257196#M7632</guid>
      <dc:creator>DerekLau</dc:creator>
      <dc:date>2013-04-09T08:02:46Z</dc:date>
    </item>
  </channel>
</rss>