<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 CodeWarrior Debugger with Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-Debugger-with-Kinetis/m-p/255331#M7503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using CodeWarrior with a TWR-K60D100M.&amp;nbsp; My project is using the Freescale compiler and the "Generate Debug Information" check box is checked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I put a breakpoint in some functions, many of the local variables are "not in scope," even though they clearly are.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to really debug, I need to look at some of these values.&amp;nbsp; Is there any way to generate better debug information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Aug 2013 18:56:48 GMT</pubDate>
    <dc:creator>mikesutton</dc:creator>
    <dc:date>2013-08-14T18:56:48Z</dc:date>
    <item>
      <title>CodeWarrior Debugger with Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-Debugger-with-Kinetis/m-p/255331#M7503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using CodeWarrior with a TWR-K60D100M.&amp;nbsp; My project is using the Freescale compiler and the "Generate Debug Information" check box is checked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I put a breakpoint in some functions, many of the local variables are "not in scope," even though they clearly are.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to really debug, I need to look at some of these values.&amp;nbsp; Is there any way to generate better debug information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2013 18:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-Debugger-with-Kinetis/m-p/255331#M7503</guid>
      <dc:creator>mikesutton</dc:creator>
      <dc:date>2013-08-14T18:56:48Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior Debugger with Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-Debugger-with-Kinetis/m-p/255332#M7504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;if you would not have debug information, then you would even not see source files/line information.&lt;/P&gt;&lt;P&gt;It seems that the compiler might have removed local variables (keeping them in registers?). If you have optimizations enabled, you can disable it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 12:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-Debugger-with-Kinetis/m-p/255332#M7504</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-08-15T12:17:43Z</dc:date>
    </item>
  </channel>
</rss>